Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L8 unresponsive when used with nRF52840

The SATEL-VL53L8CX dev boards were all out of stock, so I picked up the LS53LX-SlL8 Light Saber Sensor VL53L8CX by Gilisymo for debugging before I build my own PCB. I am interfacing with the sensor via the Adafruit itsy bitsy nRF52840 (but have also ...

joebreda by Associate
  • 2581 Views
  • 2 replies
  • 0 kudos

Resolved! X-CUBE-TOF1 I2C issue with the STM32WL

Hello, I noticed that using the X-CUBE-TOF Package with the STM32WL55JC Nucleo-Board has an issue with the I2C-Peripheral(I2C-2). This genrates the I2C code in the IDE. And the Sensor can be derived.while if I define the Sensor bus IO:The Generated c...

_legacyfs_online_stmicro_images_0693W00000binJDQAY.png _legacyfs_online_stmicro_images_0693W00000binK1QAI.png _legacyfs_online_stmicro_images_0693W00000bin7hQAA.png _legacyfs_online_stmicro_images_0693W00000binKzQAI.png
AElgh by Associate III
  • 2406 Views
  • 2 replies
  • 1 kudos

VL53L1B?

Need a help.Got VL53L1B (with a letter "B" at the end), unfortunately can't find any reference to it.Please help me recognise what is "B" suffix mean? Is it VL53L1 or VL53L1X or ...?Thanks a lot!

bodyaz by Associate II
  • 2610 Views
  • 5 replies
  • 0 kudos

Resolved! Human body detection with ToF sensor(VL53L4CX)

Hi, I'm new to the community and I hope someone could help me with the following. I was wondering is there any way to distinguish between a human body and a static object, like a piece of paper when detecting obstacles with ToF sensors(e.g. VL53L4CX,...

Gabor23 by Associate II
  • 4527 Views
  • 4 replies
  • 0 kudos

Resolved! Has anyone observed this (attached) behavior on VL53L0x?

I'm collecting 100 samples on a 200ms timing budget and reporting the average once a minute, so if it's just one sample, it's high by what you see * 100. The behavior appears sensitive to the value for sensor.setSignalRateLimit(). I have it down fro...

Martysm by Associate II
  • 5856 Views
  • 8 replies
  • 0 kudos

about VL53L1X crosstalk compensation with VL53L1X ULD driver

Dear Sir,We use VL53L1X for our application. We use a glass cover and found crosstalk problem.We try to compensate the crosstalk. There are three functions in VL53L1X ULD driver as1)VL53L1X_ERROR VL53L1X_SetXtalk(uint16_t dev, uint16_t XtalkValue);2...

DSai.1 by Associate III
  • 2495 Views
  • 5 replies
  • 0 kudos

VL53L0CXV0DH/1 issue after production

I've manufactured 160 boards implementing the VL53L0CXV0DH/1. Many work as expected but some of them (approximately 50 units) give 8191 always as a result. I've noticed that these devices should be treated carefully using a recommended reflow profile...

Gaston_0-1698267119207.png
Gaston by Senior
  • 1883 Views
  • 1 replies
  • 0 kudos

Resolved! How to operate VL53L7CX ToF in 64 zones.

Hi.Regarding the VL53L7CX, I downloaded STSW-IMG036 (API Source) from the product page and tried running the Nucleo board and sensor using the example project included there. However, the default sensor operation setting in the code is 16(4×4) zones,...

JSP by Associate II
  • 3117 Views
  • 4 replies
  • 0 kudos