Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L4CD give back a wrong ID

Hi ! I'm using the VL53L4CD sensor's example with the Nucleo-L432KC.A first problem I solved was that the VL53L4CD didn't have the adress 0x52 as in the documentation, but 0x29 (this problem has already mentioned in a topic).My current problem is tha...

CPoisson by Associate III
  • 4457 Views
  • 5 replies
  • 4 kudos

Resolved! VL53L8CX Simulation

Hi @John E KVAM and @Anne BIGOT I'm attempting to mimic the ideal operation of the VL53L8CX in simulation. I've traced out 64 rays from the sensor within the the 45x45 degrees FOV as shown. Consider the top row (underlined in black) the rays are draw...

David01_0-1704227803987.png
David01 by Associate II
  • 2013 Views
  • 3 replies
  • 0 kudos

Vl53L4CX giving status 255 in alternate cycles above 7cm

Hi,I am working on a project where I am using an array of 16 VL53L4CX to measure both the X and Y coordinate of any object in front of my sensor array. I want my loop time to be less than 50ms, so I am using 1MHz I2c clock. Currently I'm able to read...

kps98 by Associate III
  • 1428 Views
  • 1 replies
  • 1 kudos

VL53L4CX - Connecting Multiple Sensors

Hi there, I am involved in a project comprising 16x VL53L4CX Sensors, we are trying to measure and track the x and y coordinates of an object in front of the sensor array. Currently, I can read from all sensors in 33ms on average. Even though I'm usi...

isaacjack by Associate II
  • 2431 Views
  • 2 replies
  • 0 kudos

VL53L8CX firmware consumes most of the STM32 flash

Hello,I am currently working with an STM32 MCU equipped with 128KB of flash memory, alongside the X-NUCLEO-53L8A1 Time-of-Flight expansion board featuring the VL53L8CX sensor. It has come to my attention that the sensor's firmware, as defined in vl53...

Mostafa1 by Associate II
  • 2354 Views
  • 3 replies
  • 3 kudos

Vl53l8cx sharpener can not be set!

I am using the latest ULD driver of vl53l8cx. The sensor can work now. But when I use the function vl53l8cx_set_sharpener_percent to change the sharpener param, it does not work. There is no effection on the distance. I also used the vl53l5cx_set_sha...

WeiJia by Associate II
  • 2466 Views
  • 2 replies
  • 0 kudos

Raspberry Pi 4 driver for the VL5L5CX ?

I downloaded the simplified driver for the VL5L5CX from https://www.st.com/en/embedded-software/stsw-img023.html#overview .Is there a version of platform.c and platform.h for the Raspbery Pi 4?

GJoe.1 by Associate
  • 2462 Views
  • 5 replies
  • 0 kudos