Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L5CX arduino mega 2560

I just purchased the VL53L5CX-SATEL Breakout Boards for VL53L5CXhttps://estore.st.com/en/vl53l5cx-satel-cpn.htmland i have been trying unsuccessfully to get it to work with an Arduino Mega 2560. Does anyone know if it is possible to get it working wi...

rfashanu by Associate
  • 2056 Views
  • 1 replies
  • 3 kudos

Resolved! VL53L1X Duribility

I have been testing with the VL53L1X TOF sensor and am curious on the durability of the sensor in rugged environments. Such places would look like an industrial environment where vibration and impacts in inevitable. The sensor PCB would be potted and...

Resolved! ToF-Sensor to detect part distance

Hello, I'm trying to use a ToF-Sensor to track the distance of metal parts (sheets, cog wheels etc.) usually in the range of 0-60cm. The thing is that I am only interested in the distance of the surface that is directly below the sensor, the center o...

Jun by Associate
  • 2513 Views
  • 1 replies
  • 1 kudos

Resolved! VL53L8 Firmware loading

In the ULD driver for the VL53L8 is the file vl53lmz_api.c. In line 354 to 364, the firmware is loaded in pieces of 0x8000 bytes:My microcontroller has not enough ram to handle such big blocks, so I have to load the firmware in smaller pieces. But fo...

MBaum7_1-1705408412436.png
MBaum.7 by Associate III
  • 5022 Views
  • 1 replies
  • 0 kudos

Resolved! About the histogram data of VL53L8

As shown in the figure is a ball, the depth difference of one pixel is less than 3.7mm. But as shown in the histogram, the depth difference is more than 15mm. I would like to know if this is caused by noise or some other reasons? 

depth.png his.png
Licx by Associate III
  • 5678 Views
  • 10 replies
  • 0 kudos

Resolved! Using a VL53L3CX sensor with a STM32G030J6M6

I got a custom board made with these two ics and I tried to program the mcu. However, when facing FLASH and RAM size constrains I decided to remove certain parts of the library to make it fit(I removed crosstalk calibration since I don't have a cover...