Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L4CD Configuration

static const uint8_t VL53L4CD_DEFAULT_CONFIGURATION[] = {#ifdef VL53L4CD_I2C_FAST_MODE_PLUS0x12, /* 0x2d : set bit 2 and 5 to 1 for fast plus mode (1MHz I2C),else don't touch */#else0x00, /* 0x2d : set bit 2 and 5 to 1 for fast plus mode (1MHz I2C),e...

will3 by Associate III
  • 2749 Views
  • 1 replies
  • 0 kudos

Resolved! Integrating TOF and SPD with VL53L8CX - second try

(I deleted the content by accident) I'm working on a project that uses Smart Presence Detection to control a LED strip using the X-NUCLEO-53L8A1 board. I started a blank project in STM32CubeIDE and included the X-CUBE-TOF1 bundle. I have added severa...

VL53L1X Calibration reboot

Hi, We use the calibration ST APIs.  The procedure we follow is run calibration and then reboot with the new offset. However,  is there anyway to avoid having to reboot? We would like to auto calibrate in real time without a reboot if this is at all ...

will3 by Associate III
  • 2026 Views
  • 3 replies
  • 0 kudos

VL53L4CX Interface with STM32F030 DEMO Board

Hi team,I am new to the STM32 Cube IDE environment and would like to interface and control the VL53L4CX Time-of-Flight sensor using an STM32F030 DEMO Board. I kindly seek your guidance and support in achieving this.Here are the details of the hardwar...

Resolved! i2cdetect disrupts VL53L8CX operation, causing GO2 error

Hello,I am using the VL53L8CX sensor on an I2C bus, and it operates normally until I run the i2cdetect command. After running i2cdetect, the sensor stops working properly, and calling vl53l8cx_check_data_ready() returns a GO2 error status.Interesting...

Voklaif by Associate II
  • 2557 Views
  • 3 replies
  • 0 kudos

Resolved! VL53l8CX SPI not working

Hi,I am using VL53L8CX sensor from Pololu and connected it with Nucleo-F411RE board. I am using Arduino IDE 2.3 where I have downloaded STM32duino VL53L8CX library. When I run HelloWorld_I2C example with the wire  connections as mentioned with (SPI/I...

susba by Associate
  • 2702 Views
  • 2 replies
  • 0 kudos

Resolved! TOF VL53L1 Calibration Process

  Hello ST Team, We have integrated the TOF sensor into our hardware, and we would like to clarify the following: How can we calibrate the TOF sensor?When does the calibration occur—during device power-on or reboot?What are the results of the TOF sen...