2024-09-19 2:55 AM
Hi,
I am using VL53L8CX sensor from Pololu and connected it with Nucleo-F411RE board. I am using Arduino IDE 2.3 where I have downloaded STM32duino VL53L8CX library. When I run HelloWorld_I2C example with the wire connections as mentioned with (SPI/I2c-->GND, Lpn-->A3), I am getting the distance result. But when I do the same with the HelloWorld_SPI example with mentioned connection (SPI/I2c-->3v3, Lpn-->3v3), I am getting nothing. When I put the breaker in between, the initialization itself fails saying sensor initialization status 1.
I would be a great relief if you could help me with this.
Thank you
Solved! Go to Solution.
2024-09-23 3:45 PM
This problem is the same as:
2024-09-23 3:45 PM
This problem is the same as:
2025-02-04 8:42 AM
I am having the same problem here, but I know that I have the correct chips on my board (at least, the level shifters are labeled that they are both PI4ULS3V204s). After set up, it seems that the VL53L8CX's status is 0, but any calls to communicate with the sensor are left hanging, and no response is ever recieved. If anyone has SPI working with their VL53L8CX, could you share your pin assignments with me?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.