2025-01-14 3:27 PM
I’m using the VL53L8CH sensor with an ESP32 and developing a program in Arduino language based on Example_10_motion_indicator.c provided by ST. I successfully obtained the motion indicator output using a 4x4 map.
Next, I tried switching to an 8x8 map by applying the following settings:
Could you please advise if there are any additional settings required or if this might be related to a library issue? Any suggestions or insights would be greatly appreciated.
Solved! Go to Solution.
2025-02-04 1:00 AM
Hello
The reason for this is....
- The size of the Motion Indicator structure is 32 elements. This is determined by VL53L8CH firmware.
- For reference see the line "uint32_t per_aggregate_indicator_1[VL53LMZ_MI_INDICATOR_LENGTH];" in the file vl53lmz_plugin_motion_indicator.h
- Since we can't have 64 outputs from Motion Indicator we chose to reduce down from 64 to 16 to keep a regular 2x2 reduction.
- This is why in Motion Indicator mode the mi__agg_id array is mapping 64 zones to just 16 motion indicator output elements.
- Code in vl53lmz_motion_indicator_set_resolution() creates this map from 64 zones to 16 outputs.
- It is possible to use all 32 possible outputs with small changes in the vl53lmz_plugin_motion_indicator.c file. Doing this you could, for instance, have a mapping from 2x1 zones to Motion Indicator outputs
- In fact the mi__agg_id map allows a completely flexible mapping from zones to motion_indicator outputs.
Best regards
2025-02-04 1:00 AM
Hello
The reason for this is....
- The size of the Motion Indicator structure is 32 elements. This is determined by VL53L8CH firmware.
- For reference see the line "uint32_t per_aggregate_indicator_1[VL53LMZ_MI_INDICATOR_LENGTH];" in the file vl53lmz_plugin_motion_indicator.h
- Since we can't have 64 outputs from Motion Indicator we chose to reduce down from 64 to 16 to keep a regular 2x2 reduction.
- This is why in Motion Indicator mode the mi__agg_id array is mapping 64 zones to just 16 motion indicator output elements.
- Code in vl53lmz_motion_indicator_set_resolution() creates this map from 64 zones to 16 outputs.
- It is possible to use all 32 possible outputs with small changes in the vl53lmz_plugin_motion_indicator.c file. Doing this you could, for instance, have a mapping from 2x1 zones to Motion Indicator outputs
- In fact the mi__agg_id map allows a completely flexible mapping from zones to motion_indicator outputs.
Best regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.