Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Breakout Circuit for Satel-VL538

I am trying to use Satel -Vl53L8 after breaking it .  I am unable to operate it , I also tried to use the same method as used by brekout board but failed . Here is the circuit I usedIs there a way I can use the brakout board , What circuit do I need ...

Rituraj_0-1738560445285.png
Rituraj by Senior
  • 1559 Views
  • 1 replies
  • 1 kudos

Resolved! VL53L8CHV0GC/1 API/Software Reset

Hello, I am wondering if there is any software reset for the VL53L8CX when using the ST provided API. When I reprogram my micro using ST-LINK but do not do a hard power reset on my device the VL53L8CX init fails. I have attached an image below showin...

ColonelPanic_0-1738004396520.png ColonelPanic_1-1738005399379.png

Resolved! VL53L7CH API compile problem

Hello,I am trying to get my STM32WB5MM module to talk to VL53L7CH. I have working BLE project (compiles no warnings, no error and works-advertises as beacon). Now I added files from STSW-IMG043, according to doc file in the package.I also modified th...

KlemenPfce_0-1738146167507.png

Resolved! VL53L8CH registers datasheet

We are developing product with VL53L8CH integrated. Now I have to developed simple firmware that will extract data and control it and for that I need datasheet with registers description. After searching for over an hour, I cant find any datasheet, u...

VL53L3CX distance offset drifts across power cycles

Hello,in one of our new devices, we are using the VL53L3CX as a distance sensor, mainly for its small size and I2C connectivity. But we found out that even if we compensate the distance offset, after turning the device off and on again, the compensat...

VL53L5CX platform code using Raspberry Pi Pico

Hi there,I'm currently trying to write the platform code for the VL53L5CX using a Raspberry Pi Pico.I'm trying to publish the sensor data via micro-ROS in a ROS2 topic. When I use my current code I only get values close to zero and they are the same ...

vinc00 by Associate
  • 2514 Views
  • 1 replies
  • 1 kudos

Resolved! Maximum distance limit in VL53L1X

HiI want to use the VL53L1X to measure the distance of a target less than 30 cm away and about 1 cm in size.Is it possible to ignore the measurements above 30 cm?I would like to know the settings to ignore the area above 30 cm when calculating a dist...

kbsh by Associate
  • 2078 Views
  • 3 replies
  • 0 kudos

We are looking for a TOF sensor that meets some requirements

Moved  from the Feedback forum - which is not for product questions.Dear person in chargeCould you please reply to the following?Thank you so much for your attention and participation.Q1We are looking for a ToF sensor that meets the following require...

KF1 by Associate
  • 1644 Views
  • 2 replies
  • 1 kudos

Resolved! VL53L0X API download

Hello, I faced *** problem because of *** website and can't download VL53 range sensor API.It may be that I'm *** as well. But every time this *** button does nothing: https://www.st.com/en/embedded-software/stsw-img005.html#st-get-software   So ST ...

ST_Lovemachine_0-1737493778802.png

Resolved! Can a TOF sensor detect a person through a plastic case?

HI We are thinking about a method for detecting people.   The prerequisite is that we need to detect people by penetrating a plastic case with a thickness of about 3mm (white). The existing PIR cannot penetrate the case, and radar sensors are expensi...

moon1003_0-1736746444564.png
moon1003 by Associate III
  • 2700 Views
  • 3 replies
  • 3 kudos