2025-01-06 4:21 AM - last edited on 2025-01-06 4:53 AM by Andrew Neil
Hi team,
I am new to the STM32 Cube IDE environment and would like to interface and control the VL53L4CX Time-of-Flight sensor using an STM32F030 DEMO Board. I kindly seek your guidance and support in achieving this.
Here are the details of the hardware I am working with:
I would greatly appreciate any resources, sample code, or advice you can provide to help me get started.
Looking forward to your support.
Thanks and regards,
Anirudh
2025-01-06 6:17 AM
If you bought the x-nucleo-53l4a1 then just plug the board onto your nucleo. If you bought the satel-vl53l4 then there is an app note on how to hook it up.
the next bit is tricky, but let’s cheat. Download the API from the ST web site. It will be something like stsw—img0xx. Then look for the example. This example runs on the stm32-f401. But using the stm32-xcubeIDE (download from St.com) Chang the MCU. Learning the IDE is a bit of a trick. But there are tons of videos.
have fun.
2025-01-06 7:18 PM
Hi John,
Thank you for the response, but unfortunately, I only happen to have an STM32F030 DEMO Board to work with, Thus I am seeking guidance.
Additionally, is vl53l4 only compatible with Nucleo boards? Correct me if I am wrong, but if that is not the case, can you please guide me in establishing communication between STM32F030 and VL53L4CX?
I am also available to schedule a call with the ST team to discuss and resolve this. I look forward to your support.
Thanks and regards,
Anirudh
2025-02-04 1:16 AM
Hello
VL53L4 board can be used with other X-Nucleo but ST delivers only example codes for STM32F401.
To try using the STM32F030, you can use Cube-MX and remap the pins considering the UM3108.
Best regards
2025-02-05 8:28 AM
one way to do this is to start a new project using the STM32CubeIDE. Google says:
Using this you can select your board, and the code generator will build your code for you.
While building your code, you can include X-TOF and select which Time-of-flight sensor you want. This generates slightly different code. (X-ToF) is one package that controls all the ToF sensors, so it's got some arrays of function calls. But it's not that hard.
Or you can build your code without the X-Tof and then compare your project with that of the example in the API you downloaded. Merge those together, and you should be good.
There is one other thing you might try.
The example in the APi comes with an ".ioc" file. This file specifies the hardware. You might be able to just change it from the NucleoF401 board, to your board. But keep in mind, this is not guaranteed. But if your board and the F401 are close, it might just work.
- john
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.