Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Wake up microcontroller using GPIO of VL53L0X

HI folks.I would like to wake up my ESP8266 using an interrupt from the VL53L0X sensor.I have configured the sensor to use both threshold detection and to trigger an interrupt. I tested whether the interrupt is being triggered, and it is— the GPIO pi...

39425d93ebfec46a64e551e7f55199c01fbc71d4.png

Resolved! Extending the connector of the VD56G3

Hello,I am using the VD56G3 connected to a STEVAL-CAM-M0l1.  There is a very small ribbon cable between the sensor and the connector on the CAM-M0l1 - roughly 5mm.  I am working on a mock-up of some smart glasses where I'd like to extend that cable t...

dluka by Associate II
  • 1029 Views
  • 1 replies
  • 1 kudos

Resolved! vl53L4CD coverglass distance

Hi!I have a question about calibrating vl53L4CD and using a coverglass. I am doing experiments with a sample flat panel from Gilysmo, and I have noticed that if the panel is 2-3mm from the sensor, the calibration doesn't compensate for it. It looks l...

Resolved! Suggest the sensor which have range up to 15 meter.

Hello Team,                I am finding the sensor which have the up to 15 meter range.                                i am using this sensor in my water level detection project so according to suggest me the sensor.  Thanks and regard'sASHISH K.

Ashish123 by Associate II
  • 3232 Views
  • 5 replies
  • 2 kudos

Advice on VL53L7CX and very high reflective fabric

Hello everyone,We recently tested the VL53L7CX and ran across an issue with very high reflective fabrics. Here are two images of such fabric. The first is a picture taken with flash light off, second picture is taken with flash light on. From the mom...

S1M_0-1745193280050.png S1M_1-1745193318610.png
S1M by Associate II
  • 2124 Views
  • 4 replies
  • 0 kudos

Resolved! register adresses

Hi, i am trying to connect the nrf54L15 with the VL53L4CD sensor. I am having trouble with library and the code. Struggling with connecting the nrf54L15 to the sensor in the different libraries. Are you able to share the different register adresses f...

espen by Associate
  • 642 Views
  • 1 replies
  • 0 kudos

Does anyone know of a module using the VD55H1?

I know the VD55H1 is in preview phase and might be difficult to get it from ST. Although from the you tube videos it seems it is ready to be requested. Do you know what is the status to get one sensor? And if maybe is there any design house offering ...

WDela.1 by Associate II
  • 5087 Views
  • 9 replies
  • 1 kudos

Resolved! Clarification in P-NULCLEO-53L8A1A

Hi Team,We have the two boards as mentioned below.                      The Code generated in Cube MX is for the F401RETX(which configures the MCU inside VL53L8CX)In the above diagram , the host is the F401RETX . Please confirm , if our understanding...

Image(8)(1).jpeg TOF.png
Vbala.1 by Associate II
  • 1018 Views
  • 1 replies
  • 0 kudos