Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Unreasonable Data from VL53L8CX Sensor

Hello Everyone, I am currently using the vl53lmz_uld_api  tto process data measured by the VL53L8CX sensor. I have also used the "example_12_cnh_data" to retrieve data from my sensor. However, the incoming data seems completely incorrect, and I don't...

kgb by Associate III
  • 5427 Views
  • 15 replies
  • 1 kudos

Resolved! Getting data from VL53L8CX using vl53l8cx_api

Hello  everyone,  I started learning programming on the STM32 ecosystem a few weeks ago, and I'm currently trying to get data from the VL53L8CX sensor using the NUCLEO-F401RE expansion boards and the vl53l8cx_api. I wrote a small program based on wha...

kgb by Associate III
  • 1316 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L8CX: Histograms manipulation and Interpretation.

Hello Everyone,I am currently working on a project to determine if it is possible to differentiate between a glass cup and other types of cups using VL53L8CX sensor data histograms, and also to detect the fill level. I have already collected data fro...

kgb by Associate III
  • 1974 Views
  • 4 replies
  • 0 kudos

Resolved! vl53l1x sensor initialization problem

I'm using the VL53L1X in the Arduino environment. During the initialization phase, I can read the device address as 0x29, and the device ID is EACC — so there's no issue with that.However, when I try to read the register VL53L1_FIRMWARE__SYSTEM_STATU...

eneeen by Associate II
  • 1397 Views
  • 1 replies
  • 0 kudos

Resolved! Cover glass for VL53L4ED

I am putting together a water level sensor based on the vl53l4ed. The device will be in an outdoors setting with wild swings in environmental conditions. I am having hard time to design a cover / cover glass system for the TOF sensor. I have now conc...

kossiN by Associate
  • 1359 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L4CD Setup Issue

Hello, Apologies in advance for the length of this post. I am looking for some advice as I am working on getting a cpp based callback for the VL53L4CD sensor, to do this I have written a file which should perform all the same setup as the driver prov...

BruGenie by Associate II
  • 1484 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L7CX et VL53L8CX

I recently purchased a VL53L7CX and VL53L8CX, so I wanted to test the Motion Indicator functionality for each zone to show if the targets moved and how they moved via SPD of the software by STM except that there, when two people present themselves in...

Freedy by Associate II
  • 3157 Views
  • 6 replies
  • 0 kudos

Resolved! Function of INT and SYNC in VL53L8CX

Hi Team,  Could you please share the detailed function of INT and SYNC in VL53L8CXV0GC/1?  We would probably use one sensor or two. If case of one sensor SYNC input doesn't add any value to the design. If two sensor used they'll probably share the pr...

Mukeshk by Associate II
  • 2713 Views
  • 7 replies
  • 1 kudos

Problem with TOF050C-VL6180X time-of-flight (TOF) sensors

Maybe someone can help me. I bought five TOF050C-VL6180X time-of-flight (TOF) sensors, which also work with the Adafruit_VL6180X library, but they behave completely differently:Two:At a distance of 30 mm, the script shows: 0 mmAt a distance of less t...

Jwinns by Associate
  • 1040 Views
  • 1 replies
  • 0 kudos