Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! error with vd66gy on Raspberry Pi

Hello everyone, i'm trying to use the vd66gy with the raspbeery Pi x64 connected on cam0 and im following all the steps of the "Linux Start Guide for ST BrightSense" but it still doesnt work. I downloaded the drivers for the camera as well as the lib...

error_message.png inner_driver.png
aimpet by Associate II
  • 2839 Views
  • 5 replies
  • 2 kudos

Resolved! VL53L8CX Power up sequence

Hi John, Could please confirm if the slew rate requirement of VL53L8CX is satisfied in the EVM X-NUCLEO-53L8A1?  We're considering to use TI's TLV751180330PDSQR to power up the VL53L8CX sensor. But the TLV751180330PDSQR supports 11mV/µS approx. Also,...

Mukeshk_1-1745822684620.png Mukeshk_0-1745822667610.png
Mukeshk by Associate II
  • 928 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L4CD Calibration - Measurement Timing Budget

Hello ! I am calibrating a VL53L4CD ToF sensor. Is it suggested to set a large timing budget (e.g. 200 ms) for the offset and crosstalk calibrations' distance measurement process? In the distance measurement examples, the timing budget is set to 10 m...

Resolved! can't get VL53l4CX board to work

Hi,i've been posting here a few times to get a VL53L4CX to work. I've had success so far, but the latest iteration of my little PCB is really giving me troubles.When i apply power to my board (via an esp board) it stops working (the esp32 board). It ...

cyclops by Associate III
  • 1105 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L8CH Signal Width

I am guessing there is nothing that can be done about this, but I thought I'd post about it. I got the VL53L8CH because it has better bin resolution than the VL53L3CX, which I hoped to use to distinguish between objects at different ranges that are c...

Singal Spread.png
JGarrettW by Associate II
  • 1130 Views
  • 1 replies
  • 1 kudos

Resolved! How to detect Glass with vl53l8cx histogram data

Hello everyone, I am currently working with the VL53L8CX sensor to explore solutions for a specific use case. In particular, I am trying to detect glass material using the CNH (Compacted Normalized Histogram) data—more about this can be found under t...

kgb by Associate III
  • 2073 Views
  • 4 replies
  • 0 kudos

VL53L1X Custom Board Issues

Hello! I've designed a custom PCB very similar to other breakout boards on the market, because there are additional components I want to fit in a small package alongside the VL53L1X sensor. When testing my PCB, the sensor does not initialize. I've be...

Screenshot 2025-05-01 at 4.30.14 PM.png
steefCL by Associate
  • 1173 Views
  • 2 replies
  • 0 kudos