2024-01-12 7:26 AM
Hi,
Could someone please point me to where I can find the API or programming guide (which i2c reg to read the range data, which reg to set mode etc.) document for the VL53L7CH. I have looked everywhere and the only thing I can find is the ULD examples from ST. For me, these aren't very straightforward to convert into a C/C++ library :(
I would like to write a library for ESP32/Arduino to use VL53L7CH, I found a repo for VL53L8CX but I am hoping to find a bit more documentation specifically for the L7CH so I can extend the library to read the histogram on the CH version. Any help would be appreciated :)
Thanks,
Calvin
2024-01-17 5:08 AM
Hello,
We are planning to do this porting in the coming weeks. Stay tune if you want to get a release done by ST.
Meanwhile, you can find a User Manual in the STSW-IMG043_EVK package here.
There is also an article about CNH here.
Hope this helps,
Regards
Anne
2024-03-11 5:36 AM
Hi,
Any news from the porting of software for the VL53L7CH or VL53L8CH? Is that still planned? I havent found any library for reading histogram data yet, but maybe I missed it.
Best,
Paula
2024-05-07 8:02 AM
This is still planned but more likely for end of June
Sorry for the delay
2024-07-10 2:10 AM
Hi sorry if I missed it but are there any updates on this? Thank you
2024-07-10 2:45 AM
Hello
We are a bit late. The delivery has been postponed to Q3 this year.
2025-08-26 2:23 AM
Hi,
I was just wondering if this has been done yet "library for ESP32/Arduino to use VL53L7CH & VL53L8CH "
Kind regards,
Conor.
2025-08-26 2:49 AM
Hello
Yes it has been done.
You can find it here : GitHub - stm32duino/VL53L7CH: Arduino library to support the VL53L7CH artificial intelligence enabler, Time-of-Flight (ToF) 8x8 multizone sensor with 90 degrees FoV
Anne
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.