Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Running two Adafruit VL53L4CD with Arduino R4 WiFi

I've been trying to get two Adafruit VL53L4CD's to work without a multiplexer on my Arduino R4 WiFi, and am getting stuck after getting one reading. I'm largely drawing on the code discussed here, and have also changed up the bits that nh1628 discuss...

Untitled-drawing
eclemmon by Associate II
  • 1424 Views
  • 4 replies
  • 0 kudos

Resolved! Using CNH for Advanced Detection with VL53L8CH

Hi there, we recently purchased the VL53L8CH and are hoping to take advantage of its advanced capabilities for use in a small embedded product (without having to use a desktop GUI or large ST expansion board).Can you tell us more about the advanced A...

VL53L7CX Range Sigma Factor

Hi, I am currently testing the VL53L7CX ToF sensor. During my evaluation, I came across the parameter "range sigma", but I could not fully understand what it actually represents.In addition, while creating a correlation map, I noticed that the most i...

Cafko by Associate
  • 1105 Views
  • 3 replies
  • 0 kudos

VL53L5CX outdoor performance (or a suggested alternative)

I'm currently trying to use the VL53L5CX to detect motion in the range of about 1m in front of the sensor.This seems to work fine indoors - but outdoors - I don't seem to be able to get anything more than around 30cm, even with xtalk calibration, and...

zz9pa by Associate
  • 947 Views
  • 2 replies
  • 1 kudos

Resolved! VL53L4CD sleeping?

Hi,Been a while :) Seeing some odd readings after the sensor has no real changes.  After some time when a change in the sensor distance happens it "seems" to take many readings to get good readings.Is there a sleep I don't know about? What is the rec...

will3 by Associate III
  • 675 Views
  • 3 replies
  • 0 kudos

Resolved! VL53L1CB

VL53L1CB的最低投资回报率配置是 4x4?我可以将其配置为 1x1 吗? Translated : The minimum ROI configuration for the VL53L1CB is 4x4? Can I configure it as 1x1?

labubu by Associate II
  • 525 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L4CD

Hello!I am using the VL53L4CD TOF Sensor as sold by Adafruit. I am running it with the circuit patched together as described in the example file VL53L4CD_Sat_HelloWorld.ino, also with the exact code (the only change being the port number). I am using...

eclemmon by Associate II
  • 967 Views
  • 3 replies
  • 2 kudos

Resolved! VL53L8CH More CNH Bins for One CNH

Hello,I am using the 53L8A1A to evaluate the VL53L8CH with the MZAI_EVK_v1.0.1 software. For my application, I need high CNH resolution for as long a histogram as possible, but for only one histogram. Because of that, I aggregated down to one row and...

JGarrettW by Associate II
  • 1535 Views
  • 3 replies
  • 1 kudos

Resolved! Issues with VL53L3CX in Simple Ranging app

I am trying to use the VL53L3CX with an STM32G070 for water level sensing. The app is based upon the Simple Ranging example.What I am seeing is that the distance read by the sensor alternates between two values, quite far apart. The sensor is mounted...

SidPrice by Associate III
  • 1122 Views
  • 4 replies
  • 1 kudos