2025-09-10 11:29 PM
With the MCU enable BAF and Core0 / 1 /2 reset vectors are place at 0xFC0008 / 0xFC0004 / 0xFC000C, my question is how the 3 reset vector be called during power on? just be called one by one? the reference manual doesn't give clearly description; this confused me a long time.
2025-10-02 5:54 PM
Hi Long1
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards
Joe
STMicro Support
2025-10-06 4:15 AM
Hi Long1,
The BAF code enables all the cores one by one in sequence.
Regards,
Francesco
2025-12-17 7:57 AM
The boot record starts with a 16-bit signature, then the second 16-bit is a bit-mask to tell to the BAF which cores to start.
Boot record example:
0xFC0000 .long 0x00A50003
0xFC0004 .long _reset_address2 /* Core 2 reset address. */
0xFC0008 .long _reset_address0 /* Core 0 reset address. */
The "3" (b'11) in the first word (word_0) indicates to the BAF to start core_2 and core_0 using as boot address what is stored in word 1 and word 2
Note: on SPC58, core_2 is the main core (which starts first), then core_0 start after, the last core starting si core_1 (in a three core device).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.