cancel
Showing results for 
Search instead for 
Did you mean: 

TESO LIV4F - set fix rate via I2C commands

tom_anderson931
Associate

Hi all

I have a TESEO LIV4F connected to an STMF411CEU6 via I2C. I am able to read the NMEA sentences ($GNRMC etc.) at 1Hz via I2C.

I would like to set the fix rate to the maximum 10Hz as outlined in the datasheet, but i am not able to do so. In fact I am unable to get a response for any of the commands I send via I2C. I only receive the NMEA data like $GNRMC

I've read through the documentation for the LIV4F, the software manual (UM3009) says that for the firmware configuration: "The "Factory Setting" can be changed and saved at run-time using specific NMEA commands" and also gives some I2C commands, so I am led to believe this is possible.

 

Has anyone been able to configure the fix rate via I2C commands in run-time? 

 

Here is a code snippet I am using to test my board:

 

//Command message to send

//I have also tried $PSTMGETPAR,1231 and $PSTMSETPAR,1190,0.1 with and without the "\n\r" and received no responses.

static const char *cmd = "$PSTMGETPAR,1190\n\r";

 

HAL_I2C_Master_Transmit(&hi2c1, 0x3a<<1, (uint8_t *)cmd, strlen(cmd), HAL_MAX_DELAY);

 

// Wait for the response

HAL_Delay(100);

 

// Read the response (parameters or status)

uint8_t response[256];

HAL_I2C_Master_Receive(&hi2c1, 0x3a<<1, response, sizeof(response), HAL_MAX_DELAY);

 

//this is only receiving NMEA sentences like &GNRMC, not the proprietary STM command responses like //$PSTMGETPARERROR  or $PSTMSETPAR

printf("response : %s\n", response);

 

HAL_Delay(1000);

 

thanks

Tom Anderson

3 REPLIES 3
TDK
Super User

> //I have also tried $PSTMGETPAR,1231 and $PSTMSETPAR,1190,0.1 with and without the "\n\r" and received no responses.

static const char *cmd = "$PSTMGETPAR,1190\n\r";

What about the * and the checksum?

TDK_0-1734490220677.png

 

TDK_1-1734490322203.png

 

If you feel a post has answered your question, please click "Accept as Solution".

Hi TDK,

I have since tried to implement the checksum with this function (and verified with an online NMEA checksum calculator https://www.meme.au/nmea-checksum.html)

void TA_send_NMEA_command(uint8_t *command)

{

//perform the checksum calc

uint8_t checksum = 0;

for (int i = 0; i < strlen(command); i++)

{

checksum ^= command[i];

}

 

//Append the $, *, checksum, \n, \r to the command

uint8_t TxBuffer[100] = {0};

uint8_t index = 0;

 

TxBuffer[index++] = '$'; //start with $

for(int i=0; i<strlen(command); i++) //add the whole command str

{

TxBuffer[index++] = command[i];

}

TxBuffer[index++] = '*'; //add *

sprintf(&TxBuffer[index++], "%02X", checksum); // add checksum

index++;

TxBuffer[index++] = '\r'; //add \n\r

TxBuffer[index++] = '\n';

 

HAL_I2C_Master_Transmit(&hi2c1, (0x3a<<1) , TxBuffer, strlen(TxBuffer), HAL_MAX_DELAY);

}

 

With this I have sent "$PSTMGETPAR,1190*2A\r\n", "$PSTMSETPAR,1190,0.1*3D\r\n", "$PSTMGETPAR,1231*22\r\n", still with no luck.

 

Hi Tom,

To update the GNSS fix rate, the CDB register that needs to be updated is CDB-303. The command you would need to send would be the the commands shown below

$PSTMSETPAR,1303,0.1 //sets update rate to 10Hz
$PSTMSAVEPAR         //saves the values
$PSTMSRR             //software reset device for value to take effect

//to read value back after reset
$PSTMGETPAR,1303

 

To send data to LIV4F module, you can use the API as shown below in app_gnss.c

uint8_t get_update_rate[]  = "$PSTMGETPAR,1303";				
GNSS_DATA_SendCommand(&get_update_rate[0]);						

In our firmware, we do not have the code to read the response for $PSTMGETPAR. Therefore, you would need to manually add the code.

These are the changes that you would need to do,

  • NMEA_parser.h - add function declaration to read response of PSTMGETPAR
  • NMEA_parser.c - add function definition to the declaration above. (you can follow the same method as other parser functions)
  • GNSS_parser.h - modify eNMEAMsg to add the enum that should be parsed. NMEA_MSGS_NUM value to reflect the enums added

If you have a logic analyzer, could you please capture the screenshot of I2C bus when you send the data? I would like to see if the device is ACKing the data sent to it.

Thanks,

George


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.