Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Need to Flash the program every time i power up my board

Hi, I've made a custom board using an SPC5 microcontroller for my automotive-based application, but I've been facing the issue that I need to flash my code with my external SPC5 debugger every time I power up my board, and then only it starts working...

SV.9 by Associate II
  • 1995 Views
  • 1 replies
  • 1 kudos

Resolved! Flashing via CAN bus

Hi I need to flash via CAN bus and I understood it is possible using SPC5-FLASHER on PC connected to the target via USB/CAN interface with SPC5_UPDATER_CONN=SPC5_UPDATER_CONN_CAN. But I need also to flash a target from another target with SP57xx so I...

Resolved! SPC582B SPI synchronous behaviour during ISR

Hi all,I am using SPC582B mcu.The system timer is based on PIT0 CH0 (default choice) at frequency 1kHz.In the timer IRQ handler, I need to invoke SPI spi_lld_exchange API. Problem is this API doesn't complete, remaining stuck on the whileSPC5_SPI_WAI...

FPros1_0-1708968445444.png FPros1_1-1708968514255.png
FPros.1 by Associate III
  • 1997 Views
  • 1 replies
  • 0 kudos

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC58EC-DISP board in reset mode, and not able to connect to JTAG.

Hi, I have been working with the board for quite some time and everything was functioning normally. Last day, upon powering the board, I noticed that the board has entered reset mode. Also, I have been unable to establish a JTAG connection.Do you kno...

RSeba.2 by Associate III
  • 12577 Views
  • 9 replies
  • 1 kudos