Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! Motor Control Project SPC58NN

Hi Team,I am working on SPC58NN. Can someone help me in creating a motor control project in SPC5 Studio. If anyone has the documentation, Please share the link.Thanks and Regards,Akhilesh

Resolved! Motor Control SPC5

Hello Team,I am not able to generate the code for the motor control application for SPC58NN board using SPC5 Studio.Please find the below snapshot of the same.Its generating the rest of the components except the motor control 

Akhilesh30_0-1708068712729.png

Resolved! Not able to generate the Motor Control for the SPC58NN

Hello Team,I am not able to generate the code for the motor control application for SPC58NN board using SPC5 Studio.Please find the below snapshot of the same.Its generating the rest of the components except the motor control  

Akhilesh30_0-1708338484592.png

Resolved! Generate SPC5 application problem

HiI'm working with SPC570 and SPC5 Studio, version: 5.8.1 with installed the SPC5Studio patch for DMA in SPC570S DSPI lld running on Windows 11. Very often I have a problem with Generate SPC5 Application because at the end of generation (that seems t...

SPC570Sxx: Bootloader and SWT

Hi,My setup:SP570S-DISP Demo Board EvaluationuC: SPC570S50E1IDE: SPC5Studio 5.8.1I'm started from example "SPC570Sxx_RLA Bootloader Application for Discovery".I modified the example in order to have the possibility to update the firmware using both C...

LeoC by Associate II
  • 2077 Views
  • 2 replies
  • 0 kudos

Resolved! SPC5-Studio check for update problem

Hello,when running "check for updates" in SPC-Studio 6.0 I get the following error for all sites: Some sites could not be found. See the error log for more detail.Unable to read repository at http://hightec.spc5studio.com/content.xml.xz.PKIX path bui...

Resolved! SPC58X

Hello,  Does anyone have more information on the hardware/software setup regarding Application Note: AN4353. I understand the rough software architecture for how this is supposed to be implemented but I dont see anything pointing to examples or suppo...

GrayKim by Associate II
  • 2637 Views
  • 3 replies
  • 0 kudos

Resolved! StellarLink and SPC560P

Hello,Does StellarLink support SPC560P microcontrollers?Best regards.

KB.2 by Associate II
  • 1440 Views
  • 1 replies
  • 0 kudos