2020-11-13 2:34 AM
Hello community,
An automotive client that i'm working with wants to devolope his own bootloader basing on ST bootloader on SPC5 product. my mission is to validate this bootloader on SPC5 eval bord of ST.So , im asking if there is a specific HW and SW tools to validate CAN UDS bootloder. Also any documentation about CAN bootloader could help
Thinks in advance
Farmer ST engineer
Zied ben Amira
Solved! Go to Solution.
2020-11-19 7:26 AM
Hello,
open the microcontroller Reference Manual and look for Boot Assist Flash (BAF) chapter,
read the section M_CAN download protocol.
Regards,
Giuseppe
2020-11-19 7:26 AM
Hello,
open the microcontroller Reference Manual and look for Boot Assist Flash (BAF) chapter,
read the section M_CAN download protocol.
Regards,
Giuseppe
2024-02-28 8:35 AM
Thanks Giuseppe,
I was hoping there were something already done by ST ....
But ... can I configure CAN as bootloader (SPC570Sxx Firmware Updater Component) and then
I will have to create only an host application to download the firmware via CAN?
Fabio
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.