Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC5 Studio Application configuration

Dear Team,           I have some doubts about How to use SPC5 Studio Application for Enabling GPIO,UART,SPI and etc. We are developing custom board using SPC582B60E1MH00Y MCU for our application. We are new for this SPC5 Controller and Studio Applica...

Priya1 by Associate
  • 940 Views
  • 0 replies
  • 0 kudos

Resolved! SPC582B60E1 Pinout Description.

Dear STMicroelectronics Support Team, I hope this message finds you well. I am currently working on a design that incorporates the SPC582B60E1MH00Y microcontroller, and I need the detailed pinout description or any supporting documentation that outli...

Priya1 by Associate
  • 1289 Views
  • 1 replies
  • 1 kudos

Basic blink led code for SPC58EE84E7

Hello,I am using SPC58EE84E7 custom board, I am able to flash the application using JTAG debugger (stellar link), Please let me where I am going wrong as the led is not blinking.Below is the configurations that I am doing to setup the project:1. 2. B...

yashg25_0-1746704799777.png
yashg25 by Associate II
  • 1135 Views
  • 1 replies
  • 0 kudos

Resolved! Stellar Studio development software is based on SR6G7.

Hello! I want to build a simple application (such as UART messages, GPIO bit flipping, etc.), with the target being SR6G7, and run it on a custom board. For this reason, I wonder what kind of work I need to do? The StellarStudio development tool has...

Leu1 by Associate
  • 1456 Views
  • 2 replies
  • 0 kudos

SPC58NH protect RAM when reset

Hello, I'm using the SPC58NH-DISP board, and my application needs to preserve some variables across a software reset — such as when the reset button is pressed or a WDT reset occurs. My application requires a warm boot feature.When I assign a value t...

Unlock JTAG programmatically by code on SPC58

Hi, I'm developing a Bootloader for SPC58, If I full secure the micro and put its LC status as In-Field on UTEST, is there a way from the internal code (I can implement a serial command for the purpose) to unlock the JTAG? Or there is no way animore?...

GMG by Associate III
  • 1540 Views
  • 2 replies
  • 0 kudos

stellar studio

我能为此问题做些什么 似乎系统无法使用 SDKS 文件夹中的工具 Translation: "What can I do with this problem? It seems that the system cannot use the tools in the SDKS folder"  

200c99ebacd1084d0572e3e94abd71ef.png
zi_n by Associate
  • 4086 Views
  • 1 replies
  • 0 kudos

SPC5Studio SPI Generating Code for SPC574K not working

Hallo,I tried to use the DSPI_0 interface with the transfer configuration as shown in the picture, but cannot generate the necessary code with the error shown below. I could try a walkaround with byte wise frames and exchanging 4 bytes at a time but ...

grafik.png
Sir_Alee by Associate II
  • 683 Views
  • 0 replies
  • 0 kudos