Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC584B-DIS GPIO configuration and usage

Hi I'm a student, I'm trying to program for the first time a SPC584B-DIS developer board. I'm trying to set 6 pin as GPIO because I want to control 6 switches by setting the voltage to 0V for close and to 5V for open but I can't figure out how to do ...

LBona.2 by Associate II
  • 2973 Views
  • 2 replies
  • 0 kudos

Resolved! SPC560B CAN example config.

Hello Fellow,I'm working with  SPC560B-DIS and loaded the example but I couldn't find where the PIN configuration for the CAN ( for flexcan_0), please let me know where can I find those?

NSood.1 by Associate
  • 1388 Views
  • 1 replies
  • 1 kudos

Resolved! spc560 user manual

Hi All,Please share the link to download user manual for the SPC560 controller.I have searched in ST site, I didnt find it.Thanks,

Resolved! how can i programming uart interrupt(sd_lld_read)?

hello,I am using the SPC582b and SPC5stdio.I want to have interrupts run whenever I receive data.But This function is difficult because it waits until input is received (sd_lld_read, &lcd_data[bit], 1)How can I implement an uart interrupt?I need your...

BKIM.11 by Associate
  • 1866 Views
  • 1 replies
  • 0 kudos

download.spc5studio.com

Dear All ,SPC5Studio updated components are available (56,57 on 58)more information on http://download.spc5studio.com/New or updated componentsRLA 1.13.0   SPC58xHxx (cut2) :       Header file update       Add support for networking test       Add pa...

Resolved! SPC570Sxx Software Reset

Hi,My setup:SP570S-DISP Demo Board EvaluationuC: SPC570S50E1IDE: SPC5Studio 5.8.1What is the simplest way to implement a reset via software?Is there any SPC5 library function that perform software reset?Thanks,Regards

LeoC by Associate II
  • 1748 Views
  • 2 replies
  • 0 kudos

Resolved! SPC570Sxx Bootloader: Check valid application

Hi,My setup:SP570S-DISP Demo Board EvaluationuC: SPC570S50E1IDE: SPC5Studio 5.8.1I'm using example "SPC570Sxx_RLA Bootloader Application for Discovery".Function "updater_jump()" In "firmware_updater.c" file, jump to application image without checking...

LeoC by Associate II
  • 1783 Views
  • 2 replies
  • 0 kudos

Resolved! SPC570Sxx: Jump to bootloader from application

Hi,My setup:SP570S-DISP Demo Board EvaluationuC: SPC570S50E1IDE: SPC5Studio 5.8.1What is the correct way to jump from application to bootloader?Thanks,regards

LeoC by Associate II
  • 1839 Views
  • 3 replies
  • 0 kudos