Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

PIT, multiple interrupts at different times

Hello all.I'm playing around with the PIT interrupts and im finding that after setting up 3 seperate timers with different interrupt rates with the same priority setup in the IRQ Component rla. It's only constantly interrupting the PIT with the lowe...

0693W000004KBNRQA4.png
AndreasPA by Associate III
  • 1713 Views
  • 2 replies
  • 0 kudos

Resolved! Creating a new SPC5 application from Scratch

Hi,I am using a SPC570S-DISP development board, and I am trying to create a new application form that. I have tested out a few example application given in the IDE, and they work fine. Now I want to develop such an application from scratch. However, ...

NDinu.1 by Associate II
  • 2179 Views
  • 3 replies
  • 0 kudos

SPC58EC DISP not build aplications

I'm loading aplication's SPC58EC DISP, and debugging, but if I change the main.c this is the 9 problens. What it's, please?Another problem is that if I change and build the project, the changes not appearin the UDESTARTERKIT.

RPari.1 by Associate II
  • 2004 Views
  • 5 replies
  • 0 kudos

Resolved! What's the difference between c55_freegcc.a and c55_gcc.a

Good morning,I am developing a project for SPC574K2 with SPC5 studio V.6 which uses the C55 flash driver with ppc-freevle-eabi-gcc compiler. I suppose I need to use the c55_freegcc.a library, I would like to understand what is the difference from c55...

Resolved! SPC5 - functions, GTM, AutoDevKit, SPC754S

Im new into the SPC5-Studio. For the beginning it would help to have a document which shows me how to implement a Signal or sth else. For my 574s-Mcu there is just one example to let an led blink. IS there maybe a library of all Functions like toggle...

NDorn.1 by Associate II
  • 1465 Views
  • 1 replies
  • 0 kudos