Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC5-UDESTK Limited code size license

In the description for SPC5-UDESTK ,It was mentioned that '' includes a perpetual, full-feature, limited code-size (256 kBytes) license '' . I want to know that what is this limited code size(256 kBytes) license means?

0693W0000059I1yQAE.png
NDinu.1 by Associate II
  • 2932 Views
  • 5 replies
  • 1 kudos

Resolved! SPC5Studio 5.8.1 pin map editor bug

Hello, pin map editor is buggy for pins 88/89 of SPC564A80L7 and set always these pins as CAN and not eSCI when the pin map editor is opened and closed, code is generated as CAN!I have modified thse pins function then directly in the code.Thanks for ...

QPATR by Associate II
  • 1147 Views
  • 1 replies
  • 0 kudos

Resolved! CUT information for SPC574K7x

What does it mean CUT?I suppose is a CPU identification tag, but I'm not sure.I developing a project with SPC5 studio V.6.0, but I don't understand which file I must include in my project between spc574k_cut24.h and spc574k.h.I see there are some ex...

Resolved! Is there any OTA guide for the SPC582B-DIS?

I'm working on a school project where I need to use OTA in order to update my code but I can't find any documentation or example to be able to implement it in the SPC582B-DIS.

JCinc.1 by Associate
  • 1129 Views
  • 1 replies
  • 0 kudos

Resolved! TPMS pressure transducer/transmitter for TPMS?

I put this here and in MEMS and Sensors, but after browsing for a component, I'm not finding any sensor ICs for automotive TPMS systems in the category of pressure transducers/transmitters used for these systems. Is there no such ST component or am ...

TJM by Senior II
  • 1024 Views
  • 1 replies
  • 0 kudos

Resolved! GTM component for SPC574S?

I recognized that a lot of components are incompatible with my SPC574S-DISP-Board. Why? It looks like its available on the K-Version.

NDorn.1 by Associate II
  • 2027 Views
  • 3 replies
  • 0 kudos

Resolved! About SPC58 flash programming?

I would like to implement the flash programming to our JTAG tool.Are there any documents that describe OnCE module and the Nexus read/write (R/W) access block? Such as those described in AN4035. The only thing that AN4035 is inapplicable for SPC58 de...

fastfret by Associate
  • 3257 Views
  • 1 replies
  • 0 kudos

I2C Communication Protocol in SPC57S

Hi,I would like to no that does SPC57S MCUs consists with I2C communication protocol?If not what you recommend as automotive MCUs with I2C communication protocol?

NDinu.1 by Associate II
  • 1201 Views
  • 1 replies
  • 0 kudos

How to configure and generate a code in SPC5 STUDIO 6.0.0

Hi Everyone,I downloaded the latest version of SPC STUDIO 6.0.0 from the ST website in that i cannot find how to configure the GPIOs UART others and generate the Hal Drivers code and customize for our application. I seen one video in the ST website ...