2023-03-08 6:04 PM
Hi There,
I purchased an STEVAL-CCA044V1 development board to evaluate the TDA7498E device as an input source for characterising audio filters.
I configured it for MONO mode as follows:
No matter what I feed into the input (100-2000Hz, 0-3Vpk-pk) all I get on the output is a ~39kHz approximately sinusoidal oscillation. This oscillation does stop when the sytem is muted or in standby (as per the Errata), implying that something is working as expected. But it doesn't appear to be functioning as an amplifier at all.
Does anyone have experience using this eval board and have any advice as to what might be wrong here?
Thanks,
David
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.