Analog and audio

Find useful information on analog and audio applications: TDA7294-based designs, PDM to PCM noise, and SPICE models.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum board changes

Dear community member, The “Analog and audio” topic is no longer supported on the ST community. The legacy content is available only by the read-only basis. If you have any requests regarding "Analog and audio”  topics, check the alternative support ...

STA350BW功放的频�?�?�以达到40kHz�?�? Is it possible to have up to 40kHz frequency response on STA350BW amplifier?

如果通过调节STA350BW输出的LC滤波器,�?�以将频�?延伸至40kHz�?�?输入I2S采样率为192kHz。Is it possible to set the frequency response of STA350BW to up to 40kHz by having a higher cut-off frequency LC filter? The I2S input frequency is set to 192kHz.

JSun.5 by Associate
  • 1649 Views
  • 2 replies
  • 0 kudos

TDA7498E output instability on STEVAL-CCA044V1

Hi There, I purchased an STEVAL-CCA044V1 development board to evaluate the TDA7498E device as an input source for characterising audio filters. I configured it for MONO mode as follows:placed J6placed J3placed J9placed J8connected the WR/L jumpers to...

DWrig.2 by Associate
  • 1161 Views
  • 0 replies
  • 0 kudos

Not getting desired frequency from DAC output pin

Hi, am having an STM32F303K8 and using its DAC to generate a sinewave of a given frequency. Am using TIM6 update event to effect the results on the DAC periphery. AM running the APB1 bus at 16MHz, and my sinewave table has 256 samples. I set my presc...

0693W00000aHPn1QAG.png
malehakim by Associate III
  • 1652 Views
  • 2 replies
  • 0 kudos

Tda7265 mute pin problem(play dont work)

I have a problem with the following:I built the single power supply circuit which mentioned in the datasheet (second picture). I use 20.5V Vs and 2x15W 8ohm speaker for output.I measured the Mute pin(5) with multimeter and always showed me 14V.It is ...

KBarn.1 by Associate II
  • 3939 Views
  • 4 replies
  • 0 kudos

How to transmit Audio using UART.

Hi,I'm using STM32WB5MM-DK board interfaced with SPH0645LM4H I2S mic for capturing audio. I also connected a playback speaker with the setup I have mentioned. I also configured UART for transmitting the PCM data from STM32WB5MM-DK to PC. When I trans...

LR.2 by Associate III
  • 6164 Views
  • 7 replies
  • 0 kudos

Resolved! TS9222 i

Hi, Below is the design1) input voltage at inverting side is 8V with the 4.7k series connecting to inv terminal2) voltage at non inverting terminal is fixed at 3.5V.3) the difference between inputs is greater than 1V(Vid=1V). 4) My question is whethe...

KR.5 by Associate II
  • 3152 Views
  • 5 replies
  • 0 kudos

Resolved! DD-out pin on the TDA7376B

Hello everyone.what the DD-out pint is used for on the TDA7376B?Does it cancel out the channel when it detect clipping on that channel?

Y.Vosko by Associate
  • 1929 Views
  • 3 replies
  • 0 kudos