2022-10-31 9:33 AM
I'm getting an RDP error even though I'm using the -rdu command, using STM32CubeProgrammer v2.11.0 in CLI mode:
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -C port=usb1 -rdu -r32 0x08000000 0x100
-------------------------------------------------------------------
STM32CubeProgrammer v2.11.0
-------------------------------------------------------------------
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : STM32 BOOTLOADER
SN : FFFFFFFEFFFF
DFU protocol: 1.1
Board : --
Device ID : unknown
Warning: Device is under Read Out Protection
Disabling memory Read Protection...
Memory Read Protection disabled successfully
Error: RDP level is set to 1, try using Read UnProtect (-rdu) command in order to remove the Read Out Protection.
This is on a fresh unflashed STM32F042 connected to USB. Why does it seem the -rdu command works but then doesn't work?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.