2023-02-07 9:05 PM
Hello,
I am troubleshooting an issue with a provisioning and testing script using the STM32_Programmer_CLI. I get "Failed to erase memory errors" in the CLI but running (as far as I can tell) the same options in CubeIDE does not generate the same error.
It would be very helpful if I could see the CLI command in full when I run or debug on CubeIDE.
Is there such a method for doing so?
Thankyou
2023-02-13 8:40 AM
you should elavorate a bit more, what about including your script for us to see?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.