cancel
Showing results for 
Search instead for 
Did you mean: 

Per UM2237 section 1.2.4, to use the STM3210E-EVAL board in USB DFU mode, I need to install DFU driver by running the "STM32 Bootloader.bat" file. Where is the bat file and how do I run it?

PHsi.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Great!

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

The command file for Windows STM32Bootloader.bat can be found after the installation of STM32CubeProg in the installation path, i.e. normally in

C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\Drivers\DFU_Driver

By the way, when working with STM32CubeIDE, it is strongly recommended not to change the target path of the STM32CubeProg, so that the tools of STM32CubeIDE can launch the programmer.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
PHsi.1
Associate II

Hi Peter: This is exactly what I was looking for. Many thanks!!

Great!

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.