2022-12-13 1:07 AM
Hi,
I have updated STM32CubeProgrammer to version 2.12.0 and our custom External Loader is not load properly anymore. In the EL section I can read "Error: Flash loader error parsing fail" and in the log I can read "Error: Flash loader 'C:\*****/MyExternalLoader.stldr" cannot be loaded."
In 2.11.0 it worked just fine.
Do I have to change anything in my EL project (Dev_Inf.c, Loader_Src.c, linker.ld...) to work in the new version?
Thanks in advance.
Dario
Solved! Go to Solution.
2023-02-14 11:45 PM
Thank you very much Tesla, good advice, it was the structure size, all along. Since I have only 2 types of sectors in my SPI FLASH, my StorageInfo structure was only 136 bytes long instead of 200. I solved by adding 64 padding bytes. After replacing the .stldr file with the fixed one, the error is gone.
typedef struct DeviceSectors
{
unsigned long SectorNum; // Number of Sectors
unsigned long SectorSize; // Sector Size in Bytes
} device_sector_t;
struct StorageInfo
{
char DeviceName[100]; // Device Name and Description
unsigned short DeviceType; // Device Type: ONCHIP, EXT8BIT, EXT16BIT, ...
unsigned long DeviceStartAddress; // Default Device Start Address
unsigned long DeviceSize; // Total Size of Device
unsigned long PageSize; // Programming Page Size
unsigned char EraseValue; // Content of Erased Memory
device_sector_t sectors[SECTOR_NUM]; // Flash sector types
unsigned long padding[16]; // Total size of struct StorageInfo must be 200 bytes
};
2022-12-23 6:58 AM
Hello @Dario BUSONI ,
Thanks for your feedback,
Could you please specify the MCU and share the used EL for further check?
Thanks,
Sara.
2022-12-23 8:01 AM
Thank you for the answer, the MCU is a STM32G070RBTx.
I'll send the EL project in a private message.
2022-12-23 10:16 AM
Could you PM me the .STLDR, don't need the project, issues with the ELF should be more apparent. Thanks.
Perhaps with the symbols it exports, the linker script sections, or the format/content of the StorageInfo structure.
2022-12-26 4:21 AM
Hello @Dario BUSONI ,
Thanks for raising this issue to our attention,
I submitted an internal Ticket for further check, I'll keep you posted with updates.
Internal ticket number: 141953 (This is an internal tracking number and is not accessible or usable by customers).
Sara.
2023-01-02 12:31 AM
Hi,
Thank you for answering. In the V2.11.0 version the same .elf/.stldr file works fine, so those files should still be correct.
I'll PM you the .STLDR, thanks.
2023-02-14 7:48 AM
Hello @Dario BUSONI ,
After further investigation, it turns out that the parsing error is caused by a wrong StorageInfo value, it is expected to be 000000c8 and not 00000088
In previous STM32CubeProgrammer versions, corrupted external loaders were accepted, but starting from v2.12.0 a check is made to display an error when loading a faulty .stldr file.
Let me know if this solves your issue!
Sara.
2023-02-14 8:15 AM
Hello,
thanks for the update. I've looked for the value you mentioned but I'm having a hard time finding it.
Here is my storage info definition, could you help me find out where is the wrong value?
#define SPI_FLASH 7
#define SECTOR_NUM 2 // Max Number of Sector types
#define MAPPED_ADDRESS 0x90000000 // STM32CubeProgrammer shall see the memory at this address
/* This structure contains information used by ST-LINK Utility to program and erase the device */
#if defined (__ICCARM__)
__root struct StorageInfo const StorageInfo = {
#else
struct StorageInfo const StorageInfo = {
#endif
"M25P16_EVLKST8500GHxxx", // Device Name + version number
SPI_FLASH, // Device Type
MAPPED_ADDRESS, // Device Start Address
0x00200000, // Device Size in Bytes (2MBytes/16Mbits)
0x00000100, // Programming Page Size 256Bytes
0xFF, // Initial Content of Erased Memory
// Specify Size and Address of Sectors (view example below)
{
{ 0x00000020, 0x00010000 }, // Sector Num : 32 ,Sector Size: 64KBytes
{ 0x00000000, 0x00000000 } // end
}
};
2023-02-14 8:30 AM
Would be sizeof() StorageInfo structure as it gets into the .ELF (STLDR) file.
Could double check size reported in .MAP file, or reported by objcopy or fromelf dumping tools.
From .MAP of one of mine
...
.info 0x00000000 0xc8
*(.rodata.StorageInfo)
.rodata.StorageInfo
0x00000000 0xc8 out/Dev_Inf.o
0x00000000 StorageInfo
.prog 0x24000004 0x1b5c
0x24000004 . = ALIGN (0x4)
*(.text)
.text 0x24000004 0x21c c:/ct/tools/gcc49_2014q4/bin/../lib/gcc/arm-none-eabi/4.9.3/armv7e-m\libgcc.a(_arm_addsubsf3.o)
...
2023-02-14 11:45 PM
Thank you very much Tesla, good advice, it was the structure size, all along. Since I have only 2 types of sectors in my SPI FLASH, my StorageInfo structure was only 136 bytes long instead of 200. I solved by adding 64 padding bytes. After replacing the .stldr file with the fixed one, the error is gone.
typedef struct DeviceSectors
{
unsigned long SectorNum; // Number of Sectors
unsigned long SectorSize; // Sector Size in Bytes
} device_sector_t;
struct StorageInfo
{
char DeviceName[100]; // Device Name and Description
unsigned short DeviceType; // Device Type: ONCHIP, EXT8BIT, EXT16BIT, ...
unsigned long DeviceStartAddress; // Default Device Start Address
unsigned long DeviceSize; // Total Size of Device
unsigned long PageSize; // Programming Page Size
unsigned char EraseValue; // Content of Erased Memory
device_sector_t sectors[SECTOR_NUM]; // Flash sector types
unsigned long padding[16]; // Total size of struct StorageInfo must be 200 bytes
};
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.