2021-09-20 9:03 AM
The STM32L152VT6X has 384KBytes of flash memory, but the STM32CubeProgrammer detects the flash size as being 128KB. When I try to flash an image of ~170KB it fails with the error "Operation exceeds memory limits". When I flash the same image with the STLINK Utility it flashes successfully.
The first image is from the stlink utility and the second is from STM32CubeProgrammer
Solved! Go to Solution.
2021-10-08 6:52 AM
Hi @senge ,
Ok I will check and come back with updates soon.
Houda
2022-02-27 8:09 PM
Can I have the file and method to increase the flash memory for STM32L031K6 using the STM32cubeprogrammer.
2022-03-01 7:24 AM
Seems like the same issue exists for STM32F7508-DK, Is it fixed across the board for all devices or shall I need to have a file added to the DB?
2022-03-01 7:50 AM
Apt to be device unique. It is suppose to read the "FLASH SIZE" memory location in the OTP/SYSTEM area which burns in the size of flash tested. The die likely has the full complement, just untested, but probably fine.
2022-03-01 7:53 AM
What's the issue with the STM32L031K6?
The die only has 32KB of FLASH, as I recall
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.