2020-12-30 4:59 AM
Hi,
I am investigating usage of STM32CubeProgrammer API package to connect, download executables to connected STM32 MCUs.
I was going through example Visual Studio project installed with STM32CubeProgrammer available at "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\api\project\Visual Studio".
I was able to successfully compile the MSVS project successfully but while running the application, getting following error. Kindly guide to resolve the error.
'STM32CubePrgAPI.exe' (Win32): Loaded 'C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\api\lib\STM32CubePrgAPI.exe'. Symbols loaded.
'STM32CubePrgAPI.exe' (Win32): Loaded 'C:\Windows\SysWOW64\ntdll.dll'. Cannot find or open the PDB file.
'STM32CubePrgAPI.exe' (Win32): Loaded 'C:\Windows\SysWOW64\kernel32.dll'. Cannot find or open the PDB file.
'STM32CubePrgAPI.exe' (Win32): Loaded 'C:\Windows\SysWOW64\KernelBase.dll'. Cannot find or open the PDB file.
The thread 0x50c8 has exited with code -1073741701 (0xc000007b).
The thread 0x9a0 has exited with code -1073741701 (0xc000007b).
The program '[28304] STM32CubePrgAPI.exe' has exited with code -1073741701 (0xc000007b).I am using Microsoft Visual Studio Professional 2017.
Regards,
Raghavendra
2022-03-01 12:13 AM
Hi @Community member!
I don't know if it can be useful for you. A lot of time is passed away. Probably you have already checked it. But I remember that if you was compiling your project as a win32 project you had to consider that the STM32CubeProgrammer should be installed as 32 bit application. Otherwise some library that are supplied in the:
.........\STM32CubeProgrammer\api\lib
do not match with your project configuration...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.