2024-08-05 6:12 AM
It's the first time I encounter this issue so I'm not familiar with it. It happens with the command "west flash". The problem started after upgrading Zephyr to v3.6.0. Prior to that it was working. Any hints are appreciated!
usage: stm32cubeprogrammer [-h] [-d DIR] [-r RUNNER] [--skip-rebuild] [--domain DOMAIN] [-H] [--board-dir DIR] [--gdb GDB] [--openocd OPENOCD] [--openocd-search DIR]
[--elf-file FILE] [--hex-file FILE] [--bin-file FILE] [--erase] [-O TOOL_OPT] --port PORT [--frequency FREQUENCY] [--reset-mode {sw,hw,core}]
[--conn-modifiers CONN_MODIFIERS] [--cli CLI] [--use-elf]
stm32cubeprogrammer: error: argument --reset/--no-reset: ignored explicit argument 'hw'
Solved! Go to Solution.
2024-08-06 1:25 AM
Hello @xavierpacheco-eaton,
Verify if CubeProgrammer is added in the boards\st\xxxxxx\board.cmake after upgrade. If not, add
board_runner_args(stm32cubeprogrammer "--port=swd" "--reset-mode=hw")
include(${ZEPHYR_BASE}/boards/common/stm32cubeprogrammer.board.cmake)
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-08-06 1:25 AM
Hello @xavierpacheco-eaton,
Verify if CubeProgrammer is added in the boards\st\xxxxxx\board.cmake after upgrade. If not, add
board_runner_args(stm32cubeprogrammer "--port=swd" "--reset-mode=hw")
include(${ZEPHYR_BASE}/boards/common/stm32cubeprogrammer.board.cmake)
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-08-06 1:01 PM
Hi All,
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Jake
ST Support
2024-08-06 1:21 PM
The issue has been resolved. As @Sarra.S pointed out, I needed to update the following line and replace --reset with --reset-mode.
board_runner_args(stm32cubeprogrammer "--port=swd" "--reset-mode=hw")
Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.