STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32F072B USB flashing

Hello,I am doing some initial development for a device that will use the STM32F072B MCU on its Discovery board. The device will need to have the ability to be programmed over USB. The Discovery board User manual section 5.8 states that this can be do...

waratu_0-1711812618618.png waratu_1-1711812644279.png waratu_0-1711928180130.png
waratu by Associate
  • 1790 Views
  • 1 replies
  • 0 kudos

2.17 still broken dual bank STM32F767ZG

I appreciate that something has been changed in this are - I see sector numbering is being different (strange but at least different)But in the end of the day DFU upload is still broken erasing sector 0005 @: 0x08020000 done erasing sector 0006 @: 0x...

arro239 by Senior
  • 2031 Views
  • 1 replies
  • 1 kudos

.dfu files do not work after download

Hi,I'm using the STM32CubeProgrammer to program an STM105. I connect it via USB (in boot mode) and I can connect successfully. Downloading a .dfu file for the project works as well.However, after everything is complete and I unplug and reconnect the ...

MarcoP by Associate
  • 2016 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 programming via USB

I am programming USB DFU in stm32f407g disc1 but i am not able to connect it in stm32cubeprogrammer as it is showing usb port as usb1. Can anyone tell me is it anything missing?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.