2024-07-31 8:18 AM
I appreciate that something has been changed in this are - I see sector numbering is being different (strange but at least different)
But in the end of the day DFU upload is still broken
erasing sector 0005 @: 0x08020000 done erasing sector 0006 @: 0x08040000 done erasing sector 0007 @: 0x08060000 done erasing sector 24786 @: 0x08080000 done Download in Progress: ±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±± 0% 2% 4% 6% 8% 10% 12% 14% 16% 18% 20% 22% 24% 26% 28% 30% 32% 34% 36% 38% 40% 42% 44% 46% 48% 50% 52% 54% 56% 58% 60% 62% 64% 66% 68% 70% 72% 74% 76% 78% 80% 82% 84% 86% 88% 90% 92% 94% 96% 98% 100% File download complete Time elapsed during download operation: 00:00:21.193 Verifying ... Read progress: ±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±± 50% 2% 4% 6% 8% 10% 12% 14% 16% 18% 20% 22% 24% 26% 28% 30% 32% 34% 36% 38% 40% 42% 44% 46% 48% 50% 52% 54% 56% 58% 60% 62% 64% 66% 68% 70% 72% 74% 76% 78% 80% 82% 84% 86% 88% 90% 92% 94% 96% 98% 100% Error: Data mismatch found at address 0x08080000 (byte = 0x00 instead of 0x49) Error: Download verification failed
if it helps feel free to test using rusefi.bin file from https://rusefi.com/build_server/rusefi_bundle_proteus_f7.zip
2024-08-06 7:57 AM
Hello @arro239
Thank you for reporting this issue. A new internal ticket 188198 is reported to address DFU upload process.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.