2025-11-13 4:40 AM
I noticed that the V 2.20 STM32CubeProgrammer erase function doesn't work under Pop_OS!, a Linux distribution. It does however work on Windows 10. I don't think this is a logic failure within the STM32CubeProgrammer but some weird interaction with the USB Driver. Just to be clear I am using STLink on a STM32N6 evaluation board. Interesting that this function does work on a STM32h747i_disco board. Another difference is I am using an USB A to USB C cable, but all the other functions work, after erase on the Windows machine.
I have the erase under Windows workaround but it is a little inconvenient.
2025-11-13 4:46 AM
The exact error is: Error: Mass erase operation failed.Please verify flash protection
2025-11-13 5:27 AM
Did you check your user is part of the required groups (usually dialout and plugdev) ?
Does the udev rules file cover both ST-Links, which might be different versions ?
2025-11-13 7:06 AM
Yes, my user is a member of both groups. Yes, I am using the same executable V 2.20 for both the N6 and H7 processor.
2025-11-13 10:26 PM
> Yes, I am using the same executable V 2.20 for both the N6 and H7 processor.
No, that's not what I meant.
The folder /etc/udev/rules.d/ contains text files describing the devices to which the "plugdev" rules apply.
At least on my (Debian-based) distros.
Here an excerpt from "99-jlink.rules" from one of my systems :
ATTR{idProduct}=="1010", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1011", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1012", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1013", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1014", ATTR{idVendor}=="1366", MODE="666"
...
As you see, it lists several product IDs, for different JLink adapter versions in this case.
I think it's at least worth to check both that your ST-Link IDs match.
I don't know Pop-OS, but what I read it is Debian/Ubuntu-based as well, so it should be similiar.
Alternatively, you can try OpenOCD to erase/flash the STM32N6 board, which supports ST-Link as well.
2025-11-14 3:30 AM
Thank you for the clarification:
I will try the OpenOCD, good thought!
I used Gemini as an intelligent grep and it said that my 99-jlink.rules file has the rules you suggested:
Yes, your 99-jlink.rules file already contains the exact permissions suggested by the vendor.
Those lines are present in the section defining the permissions for the "[new format]" J-Link Product IDs.
Here is the matching section from the file you provided:
...
ATTR{idProduct}=="100f", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1010", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1011", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1012", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1013", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1014", ATTR{idVendor}=="1366", MODE="666"
ATTR{idProduct}=="1015", ATTR{idVendor}=="1366", MODE="666"
...Your configuration file includes these rules and many others, so no changes are necessary based on that specific suggestion.
2025-11-14 3:57 AM
I did check to see if the USB id for the STM32N6 board appeared in my 49-stlinkv3.rules and it does: SUBSYSTEMS=="usb", ATTRS{idVendor}=="0483", ATTRS{idProduct}=="3754", \
MODE="660", GROUP="plugdev", TAG+="uaccess", ENV{ID_MM_DEVICE_IGNORE}="1", \
SYMLINK+="stlinkv3_%n"
So just to reiterate, my STM32CubeProgrammer does connect to the STM32N6 board but fails on erase either mass erase or the erase prior to programming a hex file.
2025-11-17 12:03 AM
> The exact error is: Error: Mass erase operation failed.Please verify flash protection
I suppose this is not the case, the initial post implies as much.
> Another difference is I am using an USB A to USB C cable, but all the other functions work, after erase on the Windows machine.
And I suppose you have tried different cables. I have heard about such instances occasionally.
> Just to be clear I am using STLink on a STM32N6 evaluation board. Interesting that this function does work on a STM32h747i_disco board.
Another difference might be the ST-Link firmware version.
Perhaps the version on the N6 eval board requires an update.
By the way, I downloaded the JLink firmware for ST-Links from Segger's website, and converted basically all my onboard ST-Links. Not the least because I use Segger Embedded Studio, which does not support the ST-Link directly (at least the free version I use).
This process is reversible.
If all else fails you could reflash this ST-Link to a JLink, and see if it works fine with different firmware.
AFAIK the CubeProgrammer supports JLinks, but better check before ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.