STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Automate Production Programming

Hello Team,To address mass Programming of Customized board , Looking help to have Batch File / Python Script which accomplishes Following Task :1. Flash The Hex file2. Set RDP13. Read UID (96-bit ) of MCU4. Log UID and Time into CSVI tried with batch...

bsuthar by Senior
  • 1774 Views
  • 12 replies
  • 2 kudos

STM32G431 STProgrammer Writing Error

I am experiencing issues when attempting to upload the code to the MCU mentioned above on my board. I am trying to upload the code using the programmer on the STM32F407 Discovery board. It reads the chip, it erases the chip, but it does not upload th...

cereyanmhendisi_0-1763016190746.png

STM32CUBEprogrammer software bug

This software has too many bugs. Could the developers please look into the main issues? 1. If the downloader fails to connect, it spams dozens of error messages. 2. Frequent freezing, primarily when the downloader fails to connect—the software gets s...

zhaowhong by Associate III
  • 634 Views
  • 5 replies
  • 0 kudos

SensorTile.box pro not entering DFU mode on Windows

Hi,I'm having problems entering in DFU mode on Windows using a sensortile.box pro. The board doesn't even show up on device manager howerver using the same board, with the same USB cable, on the same USB port on the same PC running Ubuntu the board e...

Ig by Associate
  • 1662 Views
  • 4 replies
  • 0 kudos

Resolved! Slow programming with TrustZone

Hi,I've started working with the SBSFU example recently on an STMU585. I have noticed that flashing the sbsfu_app_init.bin file is much slower (10x maybe?) if TrustZone is enabled.My workaround has been to create a script to do a regression to RDP le...

mike5 by Associate
  • 501 Views
  • 1 replies
  • 2 kudos

how to uninstall STM32CubeProgrammer on Linux?

There is an uninstaller at ~/STMicroelectronics/STM32Cube/STM32CubeProgrammer/uninstaller/uninstaller.jarBut when I java -jar it, it just produce a log then exited, and nothing in the log actually mean anything useful.I see there is a old post about ...

A424 by Associate II
  • 9275 Views
  • 11 replies
  • 7 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.