2022-03-09 6:33 AM
Hi, I've some problem using SMT32CubeProgrammer.
i am trying to connect via uart to micro stm32g491 but i receive some error messages.
15:21:34:034 : RTS low
15:21:34:034 : DTR low
15:21:34:171 : Serial Port COM15 is successfully opened.
15:21:34:172 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
15:21:34:172 : No Init bits value is : 0
15:21:34:172 : Sending init command:
15:21:34:175 : byte 0x7F sent successfully to target
15:21:34:176 : Wait ends after 1 loop, dataready = 1, delay = 0
15:21:34:176 : Received response from target: 0x79
15:21:34:191 : Activating device: OK
15:21:34:192 : Sending GetID command and its XOR:
15:21:34:192 : byte 0x02 sent successfully to target
15:21:34:192 : byte 0xFD sent successfully to target
15:21:34:192 : Wait ends after 1 loop, dataready = 1, delay = 0
15:21:34:192 : Received response from target: 0x79
15:21:34:192 : Received 4 data bytes from target : 0x03047b7b
15:21:34:194 : Chip ID: 0x47B
15:21:34:195 : Sending Get command and its XOR:
15:21:34:195 : byte 0x00 sent successfully to target
15:21:34:195 : byte 0xFF sent successfully to target
15:21:34:195 : Wait ends after 1 loop, dataready = 1, delay = 0
15:21:34:195 : Received response from target: 0x7b
15:21:34:196 : Error: GET command not acknowledged!
15:21:34:197 : Reemission of Get command
15:21:34:197 : Sending Get command and its XOR:
15:21:34:197 : byte 0x00 sent successfully to target
15:21:34:214 : byte 0xFF sent successfully to target
15:21:34:214 : Received response from target: 0x1b
15:21:34:215 : Error: GET command not acknowledged!
15:21:34:218 : Reemission of Get command
15:21:34:218 : Sending Get command and its XOR:
15:21:34:222 : byte 0x00 sent successfully to target
15:21:34:224 : byte 0xFF sent successfully to target
15:21:34:226 : Received response from target: 0x33
15:21:34:228 : Error: GET command not acknowledged!
15:21:34:328 : UART PORT CLOSE
but if I try to communicate with the embedded bootloader of stm32 using another software (for example minicom or docklite) I can communicate correctly.
here are some messages on the serial:
09/03/2022 14:37:50.788 [TX] - 7F
09/03/2022 14:37:50.804 [RX] - 79
09/03/2022 14:37:51.966 [TX] - 02 FD
09/03/2022 14:37:51.971 [RX] - 7A 03 04 7B 3F 79
09/03/2022 14:37:53.091 [TX] - 01 FE
09/03/2022 14:37:53.094 [RX] - 79 33 00 00 7B 3F
09/03/2022 14:37:53.787 [TX] - 02 FD
09/03/2022 14:37:53.793 [RX] - 7B 3F 03 04 7B 7B 3F
09/03/2022 14:37:54.490 [TX] - 01 FE
09/03/2022 14:37:54.497 [RX] - 79 71 00 00 7B 3F
why can't i use stm32cubeprogrammer software?
Solved! Go to Solution.
2022-03-15 7:42 AM
lowering the bourate worked.
15:40:30 : RTS low
15:40:30 : DTR low
15:40:31 : Serial Port COM9 is successfully opened.
15:40:31 : Port configuration: parity = even, baudrate = 38400, data-bit = 8, stop-bit = 1.0, flow-control = off
15:40:33 : Timeout error occured while waiting for acknowledgement.
15:40:33 : Activating device: OK
15:40:33 : Board : --
15:40:33 : Chip ID: 0x479
15:40:33 : BootLoader protocol version: 3.1
15:40:33 : Response received from device: NACK
15:40:34 : Response received from device: NACK
15:40:34 : UPLOADING OPTION BYTES DATA ...
15:40:34 : Bank : 0x00
15:40:34 : Address : 0x1fff7800
15:40:34 : Size : 48 Bytes
15:40:35 : UPLOADING ...
15:40:35 : Size : 1024 Bytes
15:40:35 : Address : 0x8000000
15:40:35 : Read progress:
15:40:37 : Data read successfully
15:40:37 : Time elapsed during the read operation is: 00:00:01.498
15:40:52 : Memory Programming ...
15:40:52 : Opening and parsing file: BloodySensor.bin
15:40:52 : File : BloodySensor.bin
15:40:52 : Size : 149.54 KB
15:40:52 : Address : 0x08000000
15:40:52 : Erasing memory corresponding to segment 0:
15:40:52 : Erasing internal memory sectors [0 74]
15:40:53 : Download in Progress:
15:41:43 : File download complete
15:41:43 : Time elapsed during download operation: 00:00:51.146
2022-03-15 7:54 AM
how is it possible that the Chip ID changes according to the boudrate?
I am using the same board as when i wrote the question
2022-03-15 8:22 AM
Hi @ERazz.3 ,
No the chip ID doesn't' change according to the baudrate.
When the HW connection is not good( bad quality of cable ,long wires ...) Data cannot be exchanged correctly with Bootloader.
Lowering Baudrate can enhance the signal integrity so we read data correctly.
Hope it is clear.
Houda
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.