STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Are the erase commands in STM3CubeProgrammer broken? The transmitted commands on the UART do not match the requested functions

I currently implement my booloader (bases on the OpenBootloader) and test it against the STM32CubeProgrammer. I use v2.9.0 on Linux. Unfortunately when erasing sectors it does not send the expected command sequences. The behaviour is identical on CLI...

FBran.2 by Associate II
  • 5480 Views
  • 9 replies
  • 0 kudos

Getting "Device is under read out protection!" error when trying to program STM32F070RBT6 using USB port, Only on certain PCs

When trying to connect:When trying the same thing on a different PC (works on 3 different PCs, doesn't work on 3 other PCs). with the same IC it connects and programs with no issues.I checked the SW version of Cube programmer, on the 3 PCs that it wo...

0693W00000Kb1R2QAJ.png 0693W00000Kb1TnQAJ.png
AAlla.1 by Associate II
  • 3283 Views
  • 3 replies
  • 2 kudos

Resolved! STM32F411 Bricked after loading program

I have been programming with the STM32F411CE and I have now had this happen multiple times to different boards. Basically I program the board a few times and then all the sudden it will no longer connect. I get the following message from cubeIDE, STM...

KClos.1 by Associate II
  • 2874 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.