2021-07-15 2:09 AM
After PC boot program works fine for some time but after some time the screen is corrupted.
(also seen a completely black or a completely white screen). When clicking the pop-up windows are however OK.
2021-07-26 8:21 AM
Hello @ESore.2 and welcome to the Community :)
Please use the new release STM32CubeProgrammer 2.8.0 available in the ST web site.
Then, please keep me informed about your update.
If your issue is solved, please mark my answer as best by clicking on the "Select as Best" button. This will help other users find this solution more quickly.
Imen
2021-07-31 2:51 PM
Hi @ESore.2 ,
Please share your update and let me know if your issue is solved with latest release of CubeProgrammer.
Thanks
Imen
2021-09-15 12:41 AM
Finally I managed to update to version 2.8.0 - unfortunately the problem persists :|
I managed to see a message which was showed for a very short moment and only one time when trying to start the program
The message was something like "OpenJDP Platform binary not responding" and was in local language (so probably a windows generated message)
After a PC reboot the STM32CubeProgrammer 2.8.0 always start. If start fails it may restart after a number of retries.
In some cases it seems like the although the screen is blank, the program still reacts on mouse clicks.
Could the reason for the problem be that the OpenJDP Platform binary software does not work stable on my PC*
*) HP ProBook 470 with Intel HD Graphics 4600 / Windows 10
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.