STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer verification fails

Good morning,We have several equipments working with the STM32L4 MCU. These equipments can be programmed (using STM32CubeProgrammer) from different computers we have at our facilities.In one of this computers, we have a problem when trying to flash t...

Download verified successfully Debugger connection lost. Shutting down...

Starting server with the following options:    Persistent Mode      : Disabled    Logging Level       : 1    Listen Port Number     : 61234    Status Refresh Delay    : 15s    Verbose Mode        : Disabled    SWD Debug         : EnabledWaiting for d...

VLadd.1 by Associate II
  • 2818 Views
  • 5 replies
  • 0 kudos

STM32h747 dual flash programming via DFU class USB bootloader and Cube Programmer fails when start programming second flash bank 2

I have a bootloder - this is an application stored in the first sector in flash bank1 which at start is checking if USB is connected and going in flash update mode, otherwise is jumping to a application stored in the next flash sector.The bootloder m...

Mralt.1 by Associate
  • 876 Views
  • 1 replies
  • 0 kudos

i am stuck with my stm32 nucleo 64. the problem is that it is not responding to any of the code and i am beginner so i dont know how to solve it. the problem

I did not set anything though. I did some researches and I try some things :Change the Option Bytes in Target > Option Bytes > Read Out Protection. I don't know if it is relevant of the actual RDP state but when I open this tab, the RDP is on Level 1...

0693W00000DmkV3QAJ.jpg 0693W00000DmkUtQAJ.png
Pkuma.5 by Associate II
  • 1857 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.