2020-02-26 1:37 AM
New features
• Added the support of the graphic user interface (GUI) for the firmware upgrade service (FUS) and stack upgrade for the entire STM32WB Series
• Support of HSM V2 on all STM32 microcontrollers and microprocessors supporting SFI/SSP
Fixed issues
77015 STM32CubeProgrammer cannot connect ST-LINK without the mass storage feature. 78350 STM32CubeProgrammer issue with STM32G0 when programming binary (size 18448 bytes).
Known problems and limitations
• For the STM32L5 Series, the connection via the ST-LINK protocol is allowed only when mode is set to hotplug with TZEN=1.
• For the STM32L5 Series, the Option Byte programming GUI is not intuitive enough. Refer to the STM32L552xx and STM32L562xx advanced Arm®-based 32-bit MCUs reference manual (RM0438) for permitted accesses.
• For STM32L4Pxxx and STM32L4Qxxx devices, Option Byte programming via bootloader interfaces presents some limitations.
• For STM32H7Axxx and STM32H7Bxxx devices, Option Byte programming via bootloader interfaces (USB) presents some limitations.
• STM32L5 series programming presents limitation in macOS® when TZEN=1 and RDP=0x55.
• With some small-screen resolutions, the graphical interface of STM32CubeProgrammer presents anomalies such as inaccessible buttons.
• Display issues depending on the monitor used can occur with Linux®.
• SFIx on STM32H743/753 devices fails via the debug interface.
• SFI-HSM V2 get certificate fails with STM32L462xx devices.
• Parallel Flash programming fails in macOS® for microprocessors in the STM32MP1 Series
Link:
https://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-programmers/stm32cubeprog.html#overview
2020-07-16 8:43 AM
Hello.
I use STM32CubeProgrammer 2.4.0 on MacOS Mojave (10.14.6).
No ST-Link is detected. I tried 3 different NUCLEO-F767I (one new board).
A long time ago I had no problems with version 2.1.0.
I can do nothing, no board access and no firmware upgrade.
What is missing or wrong?
Joerg
2020-07-16 8:48 AM
Same problem with version 2.2.0 of STM32CubeProgrammer.
2020-07-17 7:18 AM
The problem was the USB cable. One data line has a defect probably.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.