2020-02-26 1:37 AM
New features
• Added the support of the graphic user interface (GUI) for the firmware upgrade service (FUS) and stack upgrade for the entire STM32WB Series
• Support of HSM V2 on all STM32 microcontrollers and microprocessors supporting SFI/SSP
Fixed issues
77015 STM32CubeProgrammer cannot connect ST-LINK without the mass storage feature. 78350 STM32CubeProgrammer issue with STM32G0 when programming binary (size 18448 bytes).
Known problems and limitations
• For the STM32L5 Series, the connection via the ST-LINK protocol is allowed only when mode is set to hotplug with TZEN=1.
• For the STM32L5 Series, the Option Byte programming GUI is not intuitive enough. Refer to the STM32L552xx and STM32L562xx advanced Arm®-based 32-bit MCUs reference manual (RM0438) for permitted accesses.
• For STM32L4Pxxx and STM32L4Qxxx devices, Option Byte programming via bootloader interfaces presents some limitations.
• For STM32H7Axxx and STM32H7Bxxx devices, Option Byte programming via bootloader interfaces (USB) presents some limitations.
• STM32L5 series programming presents limitation in macOS® when TZEN=1 and RDP=0x55.
• With some small-screen resolutions, the graphical interface of STM32CubeProgrammer presents anomalies such as inaccessible buttons.
• Display issues depending on the monitor used can occur with Linux®.
• SFIx on STM32H743/753 devices fails via the debug interface.
• SFI-HSM V2 get certificate fails with STM32L462xx devices.
• Parallel Flash programming fails in macOS® for microprocessors in the STM32MP1 Series
Link:
https://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-programmers/stm32cubeprog.html#overview
2020-02-26 1:44 AM
Is there a way to update from inside STM32CubeProgrammer?
2020-02-26 1:53 AM
78350 STM32CubeProgrammer issue with STM32G0 when programming binary (size 18448 bytes).
@Nawres GHARBI
There was a similar issue on the STM32F0 series, is it fixed as well?
2020-02-26 5:18 AM
Does it come with embedded JRE, both the installer and the runtime?
https://community.st.com/s/question/0D70X00000763nW/oracle-jre-license-impact
JW
2020-05-04 8:47 AM
Unfortunately the new version still does not work with the current Mac OS, returning "LSOpenURLsWithRole() failed with error -10810". I need STM32_Programmer_CLI
but it is not in the app file so I cannot copy it either. Using "java -jar .exe" also does not make the programmer_CLI in the Applications (it has STM32MP_SigningTool_CLI). I'm trying to port SBSFU for my MCU and it seems the scripts need this tool.
2020-06-01 10:11 PM
June 1st.
Go to the STM32CubeProg home page and you can download versions 2.2.0 or 2.3.0, but not 2.4.0.
2020-06-01 10:13 PM
Ignore. Human interface fail on my part.
2020-07-07 5:18 AM
On MacOS Catalina (10.15.5) the installer does not run because it is unverified; after manual install (java -jar S*.exe), the STM32CubeProgrammer UI refuses to run with 'java.lang.NoClassDefFoundError: javafx/application/Application'
What's missing here?
2020-07-07 5:21 AM
> What's missing here?
A well defined release process including test plan.
2020-07-07 5:40 AM
Greetings.
When to expect a version for Java 11?
On Ubuntu 20.04 with the 8 version of the problem
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.