2019-09-02 10:00 AM
2020-09-10 2:29 AM
Hi smade ,
It would help if you can provide more information. I don't believe a simple connection of the board to the cube programmer IDE could harm or block it, unless you did modify some parameters especially the option bytes...Is this the case here? and if so could you detail the steps you followed in order to help you unblock the board?
Also it will be good if you can precise what kind of message error you receive when connecting the board ( like is target not detected or halted etc...)
-Imen
2020-09-13 9:38 AM
Hi Imen,
I use ST_Link V2 for programming an debuging. So you can use STMCubeIDE or IAR to communicate with the VET6.
In configuration select ST-Link V2, SWD mode and not JTAG mode.
Hope this will help.
Benyoucef
2020-09-13 10:37 AM
Blocked? Bricked?
Do you connect NRST pin? Needed for "Connect Under Reset"
Can you connect with BOOT0 pulled HIGH?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.