2025-07-07 4:11 AM - last edited on 2025-07-09 6:45 AM by STTwo-32
Me 2, having the same issue as STM32C011 QFPN20 not able to be programmed using stlink-v2
Solved! Go to Solution.
2025-07-09 12:22 AM
Dear @STTwo-32 , thank you for prompt reply. i have sorted out the issue with my STM32C011F6U6TR (UFQFPN-20) .
It is my soldering temperature of 370 degree (using Hot Air Blower) is too high, and such temperature damages the STM32C011 microcontroller. I replace the dead chip and solder a new one by using 320 degree (Hot air), STM32C011 responds to my STlink-V2.
Ps: I am using STlinkV2 (clone one, 2x5 pins), and also genuine one (STlink v2)(2x10 pins). Both works on the newly soldered STM32C011F6U6TR (320 degree Celcius)
My Successful Setup:
Clock source: Internal HSI 48 Mhz
PA14- Boot0 pin : as SWCLK (did not add any pull-up or pull-down resistor)
PF2 - R\S\T\ pin : as ~Reset (active LOW) pin , this pin is pulled high to 3v3 using 10k resistor.
Thank you so much.
2025-07-07 4:51 AM - edited 2025-07-07 5:10 AM
Hello @DouglasKoo
Could you please send a picture of your ST-LINK V2 since some ST-LINK V2 are cloned as you can see here. also, you can have a look at this article.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-07-09 12:22 AM
Dear @STTwo-32 , thank you for prompt reply. i have sorted out the issue with my STM32C011F6U6TR (UFQFPN-20) .
It is my soldering temperature of 370 degree (using Hot Air Blower) is too high, and such temperature damages the STM32C011 microcontroller. I replace the dead chip and solder a new one by using 320 degree (Hot air), STM32C011 responds to my STlink-V2.
Ps: I am using STlinkV2 (clone one, 2x5 pins), and also genuine one (STlink v2)(2x10 pins). Both works on the newly soldered STM32C011F6U6TR (320 degree Celcius)
My Successful Setup:
Clock source: Internal HSI 48 Mhz
PA14- Boot0 pin : as SWCLK (did not add any pull-up or pull-down resistor)
PF2 - R\S\T\ pin : as ~Reset (active LOW) pin , this pin is pulled high to 3v3 using 10k resistor.
Thank you so much.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.