STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

ST_Link V3MINI and Cube programmer

Dear mr.I'm having problems with my project,Everything was working fine, but one morning I lost connection with the target unit, see attached image.I tried this with:  Two ST_Link V3MINI (I got them directly from ST)  Three different target board STM...

Micisag by Associate
  • 2485 Views
  • 3 replies
  • 0 kudos

STM32g474 processor nSWBOOT0 default option byte

We want to update the software of STM32G474 processor via uart. However, when we look at the "Pattern 14" option in the bootloader settings for this processor, the "nSWBOOT0" option byte is requested to be 1. However, we see that the default setting ...

mcelik by Associate
  • 1992 Views
  • 1 replies
  • 0 kudos

Resolved! STM32_Programmer_CLI.exe question

I have a custom board with STM32G070RB micro. I programmed the board several times for debugging in the development phase using theST-LINK//V2 in CubeIDE.Now I would like to generate a .bat file to program the boards, but I am facing some problems.My...

tabekb by Associate III
  • 18284 Views
  • 14 replies
  • 4 kudos

CubeProgrammer Static library files

Hi, I'm trying to use the cubeprogrammer api in my win32 application for firmware update. I'm able to do this, but there's a lot of .dll files that are required and it clutters the entire project. Is there any way you can provide a static .lib (code ...

Snapark by Associate
  • 1036 Views
  • 0 replies
  • 0 kudos

Stm32 programmer external loader delay

I have been using custom external loader for a long time without any problems. I noticed a problem when I tried to upload to a board without an external flash ic. I am using CLI 2.14.0. While mass erase completes in a few seconds under normal conditi...

Okeskin by Associate III
  • 1486 Views
  • 1 replies
  • 0 kudos

Resolved! CubeProgrammer reports RDP over native USB

When plugging in a device in DFU mode to a native USB port of the notebook cubeprogrammer reports:When using it over USB HUB or other port the Cubeprogrammer works fine (we never activated RDP).USBDeview shows no difference in the installed drivers. ...

0693W00000aISk7QAG.png
tguly.1 by Associate III
  • 6621 Views
  • 7 replies
  • 0 kudos

Resolved! hex (or bin) file to elf using Cube Programmer

Hi all.With build project I can obtain .bin, .hex and .elf file.I need to manipulate the file to add a CRC in determinate position. SO I use .bin (easiest), then convert in .hex and .elf file using:arm-none-eabi-objcopy -I binary -O ihex --change-sec...

TheRaprus by Associate III
  • 5715 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.