STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Problem with program not starting after reset

Hello.I am experiencing the following problem during development with STM32L4A6VGTxP.Is there any solution?[Configuration.]Custom board with STM32L4A6VGTxP microcontrollerSTM32CubeIDE v1.9.0STM32CubeProgrammer v2.13.0Firmware package STM32Cude FW_L4 ...

ma-hara by Associate II
  • 1422 Views
  • 0 replies
  • 0 kudos

Resolved! can't update STM32 Cube Programmer

Hi,when starting STM32 Cube Programmer (W64) or checking for updates I get this messageThere is "No Proxy" set in the Proxy settings and the Windows PC has internet access (browsing www works).Any ideas?Thanks,M

mha_0-1697473614723.png
mha by Associate
  • 10520 Views
  • 12 replies
  • 11 kudos

M29W128GL_STM32H7B3I-EVAL.stldr

HiIs it possible to get the Source code and project files?For the external Flash loader “M29W128GL_STM32H7B3I-EVAL.stldr”Used in the STM32CubeProgrammer.Best regardsStig

SKris.4 by Associate II
  • 890 Views
  • 0 replies
  • 1 kudos

Can't down STM32Cube Programmer

Hello,I have been trying to down the STM32Cube programmer but I reach a point where nothing happens. I have tried this on 2 different  browsers on 2 computers and the same thing happens.I go to the site https://www.st.com/en/development-tools/stm32cu...

nkyriakou_0-1702393199552.png

Resolved! Need help with programming STM32H563 using UART

I had created a project in STM32CubeIDE for the STM32H563 chip. I was able to flash it through UART1 using STM32CubeProgrammer but the code seems not executing. The code is just to toggle a LED every 500ms   int main(void) { /* USER CODE BEGIN 1 */...

Resolved! STLink V2 Not recognizing STM32CubeProgrammer?

 ST Link not recognizing STM Cube Programmer? - From screenshot you can see NO ST Link detected in serial number drop down and has no target information. I can (and did) upgrade firmware, On doing so, it's throwing following error( ST-Link device los...

Screenshot 2023-12-12 140310.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.