2023-12-09 12:45 AM
Dear mr.
I'm having problems with my project,
Everything was working fine, but one morning I lost connection with the target unit, see attached image.
I tried this with:
Two ST_Link V3MINI (I got them directly from ST)
Three different target board STM32G071 and STM32G030.
Two different PCs.
Two USB cable.
Uninstall and install SW from ST.
My configuration is no RST wire.
One of the questions- My setting is "Soft reset" but in the log I see "HWrst reset mode".
I don't remember... maybe the problem started after the ST-Link update?
Please advise.
Regards
2023-12-11 6:16 AM
Hello @Micisag,
Make sure to use latest release of STM32CubeProgrammer (2.15).
Then, please keep me informed about your result.
Imen
2023-12-12 12:16 AM
Hello Imen,
My target board STM32G071 start working after I've move USB cable from front my PC to rear(direct to MB of the PC)
Target board STM32G030 stay not working,
Yes, I've use latest STM32CubeProgrammer and ST-link FW.
Regards,
Micisag
2023-12-12 1:57 AM
Try connecting the reset pin and connect under reset mode!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.