STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32CubeProgrammer External Loader issue

I am reading a large external memory and it takes several minutes (slow bit banging SPI). To dump it to a file I have to read the memory twice because when I select "Save As" CubeProgrammer reads the default memory size (0x400) (not the 0x800000 I en...

pmachura by Associate
  • 1035 Views
  • 0 replies
  • 1 kudos

STM32CubeProgramcı

Gaggiuino projesine ait "SetupSTM32CubeProgrammer_win64" programı Hp Victus Windows 11pro bilgisayarıma yüklenemiyor. Son adımda kalır (adım 8/9).EN: The programme "SetupSTM32CubeProgrammer_win64" of the Gaggiuino project cannot be installed on my Hp...

STM32CubeProgrammer 2.15.0 released

STM32CubeProgrammer v2.15.0 release informationNew features:• Added the NOR flash memory and OTP fuse programming via USB and UART using OpenBootloader for the STM32MP13xx microprocessors• Added the support for the PMIC programming via UART for the S...

Resolved! ERORR NOT FOUND

After installing the programmer to the system and connecting it to STLINK, I encountered this NOT FOUND error. I don't know where the problem is. Also, my programmer is STLINK_V2.My second question is, when I try to install the STLINK UNITY software,...

MAHDI2 by Associate
  • 3004 Views
  • 4 replies
  • 1 kudos

STLINK-V3MINIE not recognized by Windows 10

HI,  We have designed a test fixture for a 6 panel PCB in which we use 6 individual STM programmers (STLINK-V3MINIE) and we sometimes see a problem where windows no longer recognizes one of the programmers and we can't get it back (complete system re...

RBerk.1 by Associate III
  • 1218 Views
  • 0 replies
  • 0 kudos

Resolved! Unable to erase using STM32_Programmer_CLI.exe

I am trying to erase my STM32U575 which is on a Nucleo board (U575ZI-Q) and it connected to the computer via ST-Link V3. I can erase the chip fine using the GUI STM32CubeProgrammer, but the command line method does nothing. This is the output I get w...

bpat by Associate II
  • 2651 Views
  • 4 replies
  • 1 kudos

Resolved! External flash nucleo-F746ZG with w25q128jv

Hello, I have a problem when i try to load a bin file using External flash. I created my own external flash with w25q128vj and nucleo F746ZG .When i try to load a bin file with stm32programmer its work only if the bin file is smaller than 128kb. Some...

Stlinkos by Associate II
  • 4677 Views
  • 7 replies
  • 1 kudos

DEV_TARGET_HELD_UNDER_RESET error from ST-LINK

I'm a complete newbe at directly programming STM and am learning using a Nucleo-l476RG board. When I try and run my code from STMCubeIDE I get errors failed to execute MI command and then "the system tried to join a drive to a directory on a joined d...

G0MGX by Associate
  • 16049 Views
  • 9 replies
  • 3 kudos

Resolved! How to use external loader from Visual Studio Code

Hello,I have a project that need external loader for QSPI Flash (STM32F412G-Disco board).I'm using Visual Studio Code to write code and build the project. It work fine and i can load it with STM32CubeProgrammer.For other project, without External Loa...

ANauz.1 by Senior II
  • 3697 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.