STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! I cannot connect ST-LINK/V2

I created a new board using STM32L431CBT6. The initial programming of the board was successful. However, once a program was written, I found that it couldn't be modified again. I suspected it might be related to Boot settings, so I tried changing Boo...

pic1.jpg pic2.jpg pic3-2.jpg pic3-3.jpg
YIshi.1 by Associate II
  • 10402 Views
  • 4 replies
  • 1 kudos

Resolved! rs485 half-duplex bootloader

I have an RS585 1/2 duplex transceiver hooked to USART2 configured for hardware flow control (RS485) on an STM32L412 micro.Is it possible to program a virgin part using the STM32CubeProgrammer, and to later do a firmware update over this comm channel...

FStra.9 by Associate III
  • 8053 Views
  • 10 replies
  • 1 kudos

Resolved! STM32 system bootloader UART protocol

I am developing a custom bootloader for a client on an STM32 system. I am using STM32CubeProgrammer to exercise the new bootloader and the built-in system bootloader to investigate the protocol being used over UART. In addition, I am referring to AN ...

SidPrice by Associate III
  • 2606 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeProgrammer USB programming failed

I'm using a STM32F105 and can program the firmware with an ST-Link to get firmware with USB DFU device driver on the device.The device gets recognised if I connect it with USB and I can connect and read the memory without issues.If I try to program a...

Scherm­afbeelding 2023-12-19 om 11.49.26.png
MEige.1 by Associate III
  • 9371 Views
  • 14 replies
  • 0 kudos

Resolved! STLink V3 Error

Hello, I use the original StLink V3 set, along with STM32CubeProgrammer via cmd. Sometimes I encounter an error where ST-Link jumps into Error: ST-LINK error (DEV_USB_COMM_ERR).I don't know how to resolve it. The only solution that works for me is to...

JJRR by Senior
  • 5683 Views
  • 8 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.