2024-07-03 4:02 AM
Hi,
I have executed the scripts to generate SFI on a Linux machine and I have successfully completed the process. Now, I want to run these scripts in a GitLab CI/CD pipeline to automate the process. However, when I try to execute the script, I get this error:
$ ./GenerateSFI_OEM_Dev.sh
qt.qpa.xcb: could not connect to display
Segmentation fault (core dumped)
Does anyone know how I can run these scripts in a GitLab CI/CD pipeline? For example, I want to execute this script:
#!/bin/sh # Set to the default installation path of the Cube Programmer tool # If you installed it in another location, please update path tool_dir=~/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32TrustedPackageCreator_CLI key=../Keys/aeskey.bin nonce=../Keys/nonce.bin optbyte=$tool_dir/SFI_OB_CSV_FILES/SFI_OB_U5_2M.csv binary=../Binary/OEM_Dev.bin binary_base_add=0x08000000 sfi_out_file=../Binary/OEM_Dev.sfi sudo $tool_dir -sfi -fir $binary $binary_base_add -devid 0x482 -k $key -n $nonce -ob $optbyte -v 1 --ramsize 0x55500 --token 0x80F0000 -hash 1 -o $sfi_out_file
Best regards,
2024-07-24 6:40 AM
I would also be interested in running STM32TrustedPackageCreator in a gitlab pipeline.
Interestingly, STM32TrustedPackageCreator_CLI actually links to GUI libs like Qt or X11 which makes it hardly a CMD tool.
@st pipelines are an important part of software development and export nowadays. Please make our life a bit easier when generating signed binaries in containers. Lots of people would appreciate it I think.
2024-07-29 3:54 AM
Hi,
I managed to run the STM32 Cube Programmer scripts as follows:
With this, I was able to run the scripts to generate the SFI file and install it on the microcontroller through the GitLab pipeline.
Before running the pipeline, we will need to connect the microcontroller to the Linux machine.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.