STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! DFU Firmware lost

Hi,My MCU is STM32F746ZG. When I want to use DFU to upgrade my board by STM32CubeProgrammer, It show "No DFU detected" in the port list. And I use "zadig" to try install DUF driver, it cannot find any STM DUF device, too.Do my DFU firmware lost in my...

cloud_liu by Associate II
  • 2807 Views
  • 4 replies
  • 0 kudos

STM32F103C8T6 no USB Detection

Hello,I designed a PCB with an STM32F103C8T6, and I've included the schematic below. I want to program it via USB, so I used designs I found online for the layout. The crystal is 16MHz. When I connect the USB to the computer, it detects a USB connect...

JTAPIE_0-1730897005656.png
JTAPIE by Associate II
  • 1795 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeProgrammer does not run on Fedora 41

Hello,I have installed a fresh STM32CubeProgrammer on my Fedora 41 Linux system, but I am unable to run it.After installation, I have tried running it both using the desktop menu entry and from terminal, however it never starts and crashes with the m...

Resolved! inconsistent designation of registers

In the CubeProg, (for instance) the RCC_D1CCIPR value names (*SRC) are different than in the RM 0433 (*SEL). Such things are a bit annoying, if one tries to find things by a keyword search, of if unsure about "is it really the same entity"? Can someo...

pkoevesdi_0-1730451210735.png pkoevesdi_1-1730451330120.png

Resolved! STM32 programmer failed PCB not working afterwards

 I'm trying to flash my custom STM32L152RET6 board using the command-line version of CubeProgrammer. Initially, everything seemed fine, but I wanted to ensure the firmware couldn't be read out. So, I set the option bytes with -ob RDP=1 to enable read...

mt1 by Associate II
  • 3032 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.